4.3 SAM G5x

SAM G5x Videos

Table 4-14. SAM G5x Videos
Sl. NoType/Focus AreaHardware Board/Kit UsedDescriptionLink
1Getting Started with ToolsN/AA step-by-step guide is provided below to explain the following:
  • How to Install MPLAB X IDE
  • How to Install MPLAB XC32 Compiler
  • How to install MCC
  • How to download the MPLAB Harmony Framework from the MPLAB Harmony v3 repository

MPLAB Harmony v3 is configurable through the MCC. Refer to items 3 and 4 for specific instructions for using the MCC.

How to Set-up the Tools Required to Get Started with MPLAB Harmony v3
2Getting Started with Device/KitSAM G55 Xplained Pro Evaluation Kit (ATSAMG55-XPRO)Explains how to create a simple application on the SAM E54 using MPLAB Harmony v3. This application sends a “Hello World!” string to the PC terminal.

MPLAB Harmony v3 is configurable through the MCC. Refer to items 3 and 4 for specific instructions for using the MCC.

The same example can be ported to the SAM G55 Xplained Pro Evaluation Kit (ATSAMG55-XPRO) following the same steps.

Create Your First Project with SAME54
3Getting Started with Software ToolsN/AExplains how to use the MCC Content Manager.MPLAB® Code Configurator Content Manager
4Getting Started with Software ToolsThe video covers DM320209 and EV76S68A. The same content can be replicated for the SAM G55 Xplained Pro Evaluation Kit (ATSAMG55-XPRO).Explains how to create a new MPLAB Harmony v3 project using the MCC, and shows how to migrate an MHC-based project to an MCC-based project.Getting Started with MPLAB Harmony v3 Using Code Configurator
5Getting started with SolutionsN/AIntroduces the MPLAB Harmony v3 Reference Apps package and describes its typical application types and download methods.MPLAB Harmony Reference Applications Package

SAM G5x Training Modules

Table 4-15. SAM G5x Training Modules
Sl. NoType/Focus AreaHardware Board/Kit UsedDescriptionLink
1Getting Started with Device/KitN/AShows how to create an application to get started with the SAM D5x/ E5x using the MPLAB Harmony v3 software framework.

The training module is based on the MHC, similar steps and flow can be used to create a project using the MCC.

The same example can be ported to the SAM G5x following the same steps.

Getting Started with MPLAB Harmony v3 Peripheral Libraries on SAM D5x/E5x
2Getting started with toolsN/AShows how to create a new MPLAB® Harmony v3 project using MPLAB Code Configurator (MCC) from scratch.Create a new MPLAB Harmony v3 project using MCC
3Getting started with toolsN/AShows how to open an existing project and use it with the MCC.MCC - Open an Existing MPLAB® Harmony v3 Project
4Getting started with toolsN/AShows how to install the MPLAB Code Configurator (MCC) plug in, and how to download the MPLAB Harmony v3 framework.MPLAB® Code Configurator Overview with MPLAB Harmony Content
5Getting started with toolsThis training uses the SAM D5x/E5x. The same training can be used as a reference for other MCUs.Shows how to create a new MPLAB Harmony v3 project using the MCC.Create a new MPLAB Harmony v3 project using MCC
6MigrationThis training uses the PIC32MZ EF. The same training can be used for other MCUs.Shows how to update and configure an existing MPLAB Harmony Configurator (MHC)-based MPLAB Harmony v3 project to a MPLAB Code Configurator (MCC)-based project. Update and Configure an Existing MHC-based MPLAB Harmony v3 Project to MCC-based Project

SAM G5x Virtual/On-Demand Training

SAM G5x Technical Briefs

Table 4-16. SAM G5x Technical Briefs
Sl. NoType/Focus AreaDescriptionLink
1Getting StartedTB3231: This document explains how to create a simple application on a SAM MCU using the MPLAB Harmony v3 modules. This application sends a “Hello World!” string to a console running on a computer.

Though this document is explained on one MCU, it can be ported to other MCUs.

Note: Microchip is moving from the MHC to the MCC. Refer to items 3 and 4 in the Videos table.
Link
2Getting StartedTB3232: This document explains how to set up the tools required to get started with the MPLAB Harmony v3 software development framework.Link
3Getting StartedTB3304: How to Add a New Configuration to an Existing MPLAB Harmony v3 ProjectLink
4Getting StartedTB3305: How to Use the MPLAB Harmony v3 Project Manifest FeatureLink
5Getting StartedTB3290: MPLAB Harmony v3 Synchronous Drivers and Their Usage in FreeRTOS Based ApplicationsLink
6Getting StartedTB3269: The Differences Between MPLAB Harmony v3 Synchronous and Asynchronous Drivers and When to Use ThemLink
7Getting StartedTB3291: The Difference Between MPLAB Harmony v3 PLIBs and Drivers, and When to Use Them Link
8Getting StartedTB3253: How to Build an Application by Adding a New PLIB, Driver, or Middleware to an Existing MPLAB Harmony v3 ProjectLink
9Getting StartedTB3246: How to Use the MPLAB Harmony v3 Debug System ServiceLink
10Peripheral FeatureTB3230: Various Timers on SAM DevicesLink
11Peripheral FeatureTB3222: EEPROM Emulation for Flash-Only DevicesLink
12MCU FeatureTB3183: What is Sleepwalking? How it helps to reduce the power consumption?Link
13Peripheral TB3181: What is TWI? How to configure the TWI for I2C CommunicationLink
14Peripheral FeatureTB3367: ADC Sequencing Using DMA and EVENT System on PIC32C and SAM MCUs Using MPLAB Harmony v3 and MCCLink

SAM G5x Application Notes

Table 4-17. SAM G5x Application Notes
Sl. NoType/Focus Area DescriptionLink
1MigrationAN4495: MPLAB Harmony v3 Project Migration application note discusses the migration of an existing MPLAB Harmony v3- based project developed on a particular hardware (microcontroller or development board) platform to another one of Microchip's 32-bit hardware platforms of the user's choice.Link
2Feature specificAN4383: 32-bit Microcontroller Wafer-Level Chip-Scale Package (WLCSP)Link
3MigrationAN3346: Introduction to MPLAB Harmony v3 for Atmel Studio and ASF UsersLink
4Peripheral FeatureAN5807: SERCOM USART on Microchip Cortex Devices (SAM and PIC32C)Link

SAM G5x Application Demonstrations

More application demonstrations are available at Microchip's MPLAB Harmony v3 GitHub repositories. Refer to the following link:

SAM G5x Reference Designs/Solutions

Table 4-18. SAM G5x Reference Designs/Solutions
Sl. NoTypeHardware Board/Kit UsedDescriptionLink
1AudioSAM G55 Audio Curiosity Development Board (EV78Y10A)SAM G55 Audio Curiosity Development BoardLink