4.2 SAM D5x/E5x
Click the following links to check various collaterals:
SAM D5x/E5x Videos
| Sl. No | Type/Focus Area | Hardware Board/Kit Used | Description | Link |
|---|---|---|---|---|
| 1 | Getting Started with Tools | N/A | A step-by-step guide is provided
below to explain the following:
MPLAB Harmony v3 is configurable through the MCC. Refer to items 6 and 7 for specific instructions to use the MCC. | How to Set-up the Tools Required to Get Started with MPLAB Harmony v3 |
| 2 | Getting Started with Device/Kit | SAM E54 Xplained Pro Evaluation Kit (ATSAME54-XPRO) | This video introduces Arm Cortex-M4 based SAM E54 Xplained Pro Evaluation Kit using MPLAB Code Configurator (MCC). The application reads room temperature from the I/O1 Xplained Pro Extension Kit every 500 milliseconds, displaying it on a serial console and toggling an LED. | Create Your First Project with SAME54 |
| 3 | Getting Started with Device/Kit | SAM E51 Curiosity Nano Evaluation Kit (EV76S68A) | Explains how to create a simple
application for the SAM E51 using MPLAB Harmony v3. This application
toggles an LED periodically and prints the LED toggling rate on a
serial terminal. Microchip is moving from the MHC to MCC. Refer to items 6 and 7 in the table. | Getting Started with SAM E51 Curiosity Nano |
| 4 | IoT | SAM E51 Curiosity Nano Evaluation Kit (EV76S68A) | Explains the steps to Create an
IoT-Based Heart Rate Monitoring Application. The application displays heart rate readings (in beats per minute (bpm)) on a very low-power consuming display and posts this Heart Rate data to the Microchip Bluetooth Data (MBD) Android™ mobile application through Bluetooth Low Energy. | How to Create a BLE Fitness Tracker Application on SAM E51 Curiosity Nano |
| 5 | Getting Started with Device/Kit | SAM E54 Curiosity Ultra Development Board (DM320210) | Explains how to create a simple
application for the SAM E51 using MPLAB Harmony v3. This application
toggles an LED periodically and prints the LED toggling rate on a
serial terminal. The demonstration application has additional functionality to print the current room temperature using an on-board temperature sensor. | Getting Started with the SAM E54 Curiosity Ultra |
| 6 | Getting Started with Software Tools | N/A | Explains how to use the MCC Content Manager. | MPLAB® Code Configurator Content Manager |
| 7 | Getting Started with Software Tools | Video covers Curiosity PIC32MZ EF
2.0 Development Board (DM320209) and SAM E51 Curiosity Nano Evaluation Kit (EV76S68A) | Explains how to create a new MPLAB Harmony v3 project using the MCC and shows how to migrate an MHC-based project to an MCC based project. | Getting Started with MPLAB Harmony v3 Using MCC |
| 8 | Getting started with Solutions | N/A | Introduces the MPLAB Harmony v3 Reference Apps package and describes its typical application types and download methods. | MPLAB Harmony Reference Applications Package |
| 9 | CAN USB bridge and CAN-based Host/Bootloader Application using SAM E54 Xplained Pro Evaluation Kit | SAM E54 Xplained Pro Evaluation Kit (ATSAME54-XPRO) | This application acts as a CAN-USB bridge and a CAN-based Non-Volatile Memory (NVM) bootloader host application. With CAN-USB bridge functionality, it reads the data transmitted on a CAN network through the CAN peripheral and displays it on the PC serial terminal window using the USB CDC virtual COM port. With CAN NVM bootloader host functionality, it sends the binary image from the Python script to the target over the CAN bus for programming. | CAN USB bridge & CAN-based Host/Bootloader Application using SAM E54 Xplained Pro Eval Kit |
SAM D5x/E5x Training Modules
| Sl. No | Type/Focus Area | Hardware Board/Kit Used | Description | Link |
|---|---|---|---|---|
| 1 | Getting Started with Device/Kit | SAM E54 Xplained Pro Evaluation Kit (ATSAME54-XPRO) | Shows how to create an application to get started with the SAM D5x/ E5x using the MPLAB Harmony v3 software framework. | Getting Started with MPLAB Harmony v3 Peripheral Libraries on SAM D5x/E5x |
| 2 | Getting Started with Device/Kit | SAM E54 Xplained Pro Evaluation Kit (ATSAME54-XPRO) | Shows how to create an application to get started with the SAM E5x using the MPLAB Harmony v3 software framework with FreeRTOS. | Getting Started with MPLAB Harmony v3 Drivers on SAM E54 MCUs Using FreeRTOS |
| 3 | Getting started with tools | N/A | Shows how to create a new MPLAB Harmony v3 project using MPLAB Code Configurator (MCC) from scratch. | Create a new MPLAB Harmony v3 project using MCC |
| 4 | Getting started with tools | N/A | Shows how to open an existing project and use it with the MCC. | MCC - Open an Existing MPLAB® Harmony v3 Project |
| 5 | Getting started with tools | N/A | Shows how to install the MPLAB Code Configurator (MCC) plug in, and how to download the MPLAB Harmony v3 framework. | MPLAB® Code Configurator Overview with MPLAB Harmony Content |
| 6 | Getting started with tools | SAM E51 Curiosity Nano Evaluation Kit (EV76S68A) | Shows how to create a new MPLAB Harmony v3 project using the MCC. | Create a new MPLAB Harmony v3 project using MCC |
| 7 | Application Specific | SAM E54 Xplained Pro Evaluation Kit (ATSAME54-XPRO) | Shows how to create a low-power application on a SAM E54 showcasing the current measurement on Idle and Standby Sleep modes. The current consumption data is shown on a data visualizer. | Low Power Application on SAM E54 |
| 8 | Migration | Though this training is using PIC32MZ EF, the same training can be used for other MCUs | Shows how to update and configure an existing MPLAB Harmony Configurator (MHC)-based MPLAB Harmony v3 project to a MPLAB Code Configurator (MCC)-based project. | Update and Configure an Existing MHC-based MPLAB Harmony v3 Project to MCC-based Project |
| 9 | AI/ML | Integrated Graphics and Touch (IGAT) Curiosity Evaluation Kit (EV14C17A) | Shows how to create an Artificial Intelligence/Machine Learning (AI/ML) application using TensorFlow Lite for Microcontrollers (TFLM) to recognize handwritten digits on a SAM E51 Integrated Graphics and Touch (IGAT) Curiosity Evaluation Kit. | Digit Recognition AI/ML Application on SAM E51 IGAT |
| 10 | Motor control | dsPICDEM MCLV-2 Development Board
Low Voltage (DM330021-2) and ATSAME54 Motor Control Plug In Module (MA320207) | Shows how to create a motor control application Brushless DC (BLDC) block commutation using a hall sensor on a SAM E54 microcontroller. | Create your first Motor Control Application |
| 11 | IoT | SAM E51 Curiosity Nano Evaluation Kit (EV76S68A) | Shows how to develop an application
prototype from a concept without designing a Printed Circuit Board
(PCB) using the 32-bit MCU-based Curiosity Nano Evaluation Kits and
Nano base board. This training uses the PIC32CM MC00 Curiosity Nano. The same training can be used for other MCUs that are supported on the Curiosity Nano platform. | Rapid prototyping with 32-bit MCU-based Curiosity Nano |
SAM D5x/E5x Virtual/On-Demand Training
Some of the following virtual trainings were developed using other MCUs. The same trainings can be ported to the SAM E51 Curiosity Nano Evaluation Kit.
| Sl. No | Event | Description | Link |
|---|---|---|---|
| 1 | Design Week 2022 - Rapid Prototyping Connected Applications With 32-bit Microcontrollers | Discusses how to rapidly develop an IoT-centered smart appliance control application prototype from a concept. Refer to items 2, 3, 4, 5, and 6 in this table for details. | Link |
| 2 | Rapid Prototyping with Curiosity Nano: Part I webinar | Discusses how to rapidly develop an
IoT-centered smart appliance control application prototype from a
concept. In the first part, The concept of creating a system to
capture sensor data and control actuators through an I2C
interface is explained. This demonstration was developed on the PIC32CM MC00 Curiosity Nano Evaluation Kit. It can be easily ported to the SAM E51 Curiosity Nano Evaluation Kit (EV76S68A). | Link |
| 3 | Rapid Prototyping with Curiosity Nano: Part II webinar | Discusses how to rapidly develop an
IoT-centered smart appliance control application prototype from a
concept. In the second part, the concept of creating a system to
capture and display sensor data through the UART and SPI interfaces
is explained. This demonstration was developed on the PIC32CM MC00 Curiosity Nano Evaluation Kit. It can be easily ported to the SAM E51 Curiosity Nano Evaluation Kit (EV76S68A). | Link |
| 4 | Rapid Prototyping with Curiosity Nano: Part III webinar | Discusses how to rapidly develop an
IoT-centered smart appliance control application prototype from a
concept. In the third part, the concepts needed to add more
functionality to the project created in the first part of this
webinar series is explained:
This demonstration was developed on the PIC32CM MC00 Curiosity Nano Evaluation Kit. It can be easily ported to the SAM E51 Curiosity Nano Evaluation Kit (EV76S68A). | Link |
| 5 | Develop 32-bit MCU applications using MPLAB Harmony v3 | Discusses the fundamentals of MPLAB Harmony v3, the middleware, and other design tools available for application development. It showcases a weather station demonstration using the SAM D21 32-bit microcontroller using the SAM D21 Curiosity Nano (DM320119). The same can be ported for the SAM E51 Curiosity Nano Evaluation Kit (EV76S68A). | Link |
More virtual trainings are available at Microchip University. Click the following links for more details:
- Introduction To MPLAB® X IDE
- MPLAB® X IDE Tips and Tricks
- Overview of the Microchip Code Configurator (MCC) Content Manager (CM)
- Arm® Cortex®-M Architecture Overview
- Getting Started with Writing Code for the Microchip Arm® Cortex® Microcontrollers
- MPLAB® Harmony v3 Fundamentals
- Simple Applications Using the MPLAB® Harmony v3 Peripheral Libraries
- Creating Advanced Embedded Applications with 32-bit MCUs/MPUs using the MPLAB® Harmony v3 Software Framework
- FreeRTOS Simplified: A Beginner's Guide to Develop and Debug FreeRTOS Applications
- Introduction to Functional Safety
- Class B Diagnostic Libraries For Functional Safety
- Get Started Simplifying Your IoT Design with Azure RTOS
- Build and manage an IoT device with the Microsoft Azure IoT service and the Microchip SAME54 Xplained Pro evaluation kit
SAM D5x/E5x Technical Briefs
| Sl. No | Type/Focus Area | Description | Link |
|---|---|---|---|
| 1 | Getting Started | TB3231: This document explains how to
create a simple application on a SAM MCU using the MPLAB Harmony v3
modules. This application sends a “Hello World!” string to a console
running on a computer. This document is explained on one MCU, and it can be ported for other MCUs. Note: Microchip is
moving from the MHC to the MCC. Refer to items 6 and 7 in the
Videos table. | Link |
| 2 | Getting Started | TB3232: This document explains how to set up the tools required to get started with the MPLAB Harmony v3 software development framework. | Link |
| 3 | Getting Started | TB3304: How to Add a New Configuration to an Existing MPLAB Harmony v3 Project | Link |
| 4 | Getting Started | TB3305: How to Use the MPLAB Harmony v3 Project Manifest Feature | Link |
| 5 | Getting Started | TB3290: MPLAB Harmony v3 Synchronous Drivers and Their Usage in FreeRTOS Based Applications | Link |
| 6 | Getting Started | TB3269: The Differences Between MPLAB Harmony v3 Synchronous and Asynchronous Drivers and When to Use Them | Link |
| 7 | Getting Started | TB3291: The Difference Between MPLAB Harmony v3 PLIBs and Drivers, and When to Use Them | Link |
| 8 | Getting Started | TB3226: Clock System Configuration and Usage on SAM E5x (Cortex M4) Devices | Link |
| 9 | Migration | TB3298: How to Move an Application into a Desired Flash Memory Location with the Help of Linker Script on SAM E54 | Link |
| 10 | Getting Started | TB3253: How to Build an Application by Adding a New PLIB, Driver, or Middleware to an Existing MPLAB Harmony v3 Project | Link |
| 11 | Getting Started | TB3246: How to Use the MPLAB Harmony v3 Debug System Service | Link |
| 12 | Peripheral Feature | TB3230: Various Timers on SAM Devices | Link |
| 13 | Peripheral Feature | TB3222: EEPROM Emulation for Flash-Only Devices | Link |
| 14 | MCU Feature | TB3183: What is Sleepwalking? How it helps to reduce the power consumption? | Link |
| 15 | Getting Started | TB3355: How to Use the MPLAB Data Visualizer with 32-bit MCU based Curiosity Nano Evaluation Kits | Link |
| 16 | Peripheral Feature | TB3367: ADC Sequencing Using DMA and EVENT System on PIC32C and SAM MCUs Using MPLAB Harmony v3 and MCC | Link |
SAM D5x/E5x Application Notes
| Sl. No | Type/Focus Area | Description | Note Link |
|---|---|---|---|
| 1 | Migration | AN4495: MPLAB Harmony v3 Project Migration application note discusses the migration of an existing MPLAB Harmony v3-based project developed on a particular hardware (microcontroller or development board) platform to another one of Microchip's 32-bit hardware platforms of the user's choice. | Link |
| 2 | TCP/IP | AN4833: File Transfer Protocol Using MPLAB Harmony v3 TCP/IP Stack for SAM E54 MCU | Link |
| 3 | Security | AN3923: AES Cipher Modes Using MPLAB Harmony v3 for the SAM E54 | Link |
| 4 | Bootloader | AN3767: Live Update Application on SAM E54 MCU Using MPLAB Harmony v3 | Link |
| 5 | Bootloader | AN3508: Dual- Bank Bootloader on SAM E54 Microcontroller (MCU) Using MPLAB Harmony v3 | Link |
| 6 | Low-Power | AN3342: SleepWalking with Event System Using the SAM E54 | Link |
| 7 | Feature specific | AN4383: 32-bit Microcontroller Wafer-Level Chip-Scale Package (WLCSP) | Link |
| 8 | Migration | AN3346: Introduction to MPLAB and Harmony v3 for Atmel Studio and ASF Users | Link |
| 9 | Peripheral Feature | AN5807: SERCOM USART on Microchip Cortex Devices (SAM and PIC32C) | Link |
| 10 | Migration | AN5893: Migration Guide from SAM D5x/E5x to PIC32CK SG01/ SG00/GC01/GC00 | Link |
SAM D5x/E5x Application Demonstrations
| Sl. No | Type | Hardware Board/Kit Used | Description | Link |
|---|---|---|---|---|
| 1 | Getting started | SAM E51 Curiosity Nano Evaluation Kit (EV76S68A) | Getting Started Application on the SAM E51 Curiosity Nano Evaluation Kit. | Link |
| 2 | Getting started | SAM E54 Xplained Pro Evaluation Kit (ATSAME54-XPRO) | Getting Started Application on the SAM E54 Xplained Pro Evaluation Kit. | Link |
| 3 | Getting started | SAM E54 Curiosity Ultra Development Board (DM320210) | Getting Started Application with the SAM E54 Curiosity Ultra Development Board. | Link |
| 4 | IoT | SAM E51 Curiosity Nano Evaluation Kit (EV76S68A) | BLE Fitness Tracker Application on the SAM E51 Curiosity Nano Evaluation Kit and Nano Base for Click boards. | Link |
| 5 | Low-Power | SAM E51 Curiosity Nano Evaluation Kit (EV76S68A) | Low-Power Application Demonstration on the SAM E51 Curiosity Nano Evaluation Kit with OLED C. | Link |
| 6 | IoT, Automation | SAM E51 Curiosity Nano Evaluation Kit (EV76S68A) | Weather Click Example. | Link |
| 7 | HMI | SAM E51 Curiosity Nano Evaluation Kit (EV76S68A) | Eink Display Bundle Click Example. | Link |
| 8 | IoT, Medical | SAM E51 Curiosity Nano Evaluation Kit (EV76S68A) | Heart Rate 9 Click Example. | Link |
| 9 | IoT, Automation | SAM E51 Curiosity Nano Evaluation Kit (EV76S68A) | IR Thermo 2 Click Example. | Link |
| 10 | IoT, Automation | SAM E51 Curiosity Nano Evaluation Kit (EV76S68A) | 10DOF Click Example. | Link |
| 11 | Display | SAM E51 Curiosity Nano Evaluation Kit (EV76S68A) | LED Driver 3 Click Example. | Link |
| 12 | Storage | SAM E51 Curiosity Nano Evaluation Kit (EV76S68A) | EEPROM 4 Click Example. | Link |
| 13 | Gaming | SAM E51 Curiosity Nano Evaluation Kit (EV76S68A) | Thumbstick Click Example. | Link |
| 14 | Click Extension | SAM E51 Curiosity Nano Evaluation Kit (EV76S68A) | XPRO Adapter Click Example. | Link |
| 15 | IoT, Automation | SAM E51 Curiosity Nano Evaluation Kit (EV76S68A) | Fan Click Example. | Link |
| 16 | IoT, Automation | SAM E51 Curiosity Nano Evaluation Kit (EV76S68A) | GSM GPS Click Example. | Link |
| 17 | IoT, Automation | SAM E51 Curiosity Nano Evaluation Kit (EV76S68A) | PIR Click Example. | Link |
| 18 | Connectivity | SAM E51 Curiosity Nano Evaluation Kit (EV76S68A) | USB UART Click Example. | Link |
| 19 | Display | SAM E51 Curiosity Nano Evaluation Kit (EV76S68A) | OLED C Click Example. | Link |
| 20 | IoT, Automation | SAM E51 Curiosity Nano Evaluation Kit (EV76S68A) | WIFI 7 Click Example. | Link |
| 21 | IoT, Automation | SAM E51 Curiosity Nano Evaluation Kit (EV76S68A) | RFID Click Example. | Link |
| 22 | Connectivity | SAM E51 Curiosity Nano Evaluation Kit (EV76S68A) | USB I2C Click Example. | Link |
| 23 | IoT, Automation | SAM E51 Curiosity Nano Evaluation Kit (EV76S68A) | BLE 2 Click Example. | Link |
| 24 | Automation | SAM E51 Curiosity Nano Evaluation Kit (EV76S68A) | GRID EYE Click Example. | Link |
| 25 | Wireless Connectivity | SAM E51 Curiosity Nano Evaluation Kit (EV76S68A) | LR Click Example. | Link |
| 26 | Connectivity | SAM E51 Curiosity Nano Evaluation Kit (EV76S68A) | USB SPI Click Example. | Link |
| 27 | Automotive | SAM E54 Xplained Pro Evaluation Kit (ATSAME54-XPRO) | CAN to USB bridge Application using the SAM E54 Xplained Pro Evaluation Kit. | Link |
| 28 | Consumer | SAM E54 Xplained Pro Evaluation Kit (ATSAME54-XPRO) | Vending Machine Application Demonstration on the SAM E54 Xplained Pro Evaluation Kit using MP. | Link |
| 29 | Low-Power | SAM E54 Xplained Pro Evaluation Kit (ATSAME54-XPRO) | Low-Power Application on the SAM E54 Xplained Pro Evaluation Kit. | Link |
| 30 | Low-Power | SAM E54 Xplained Pro Evaluation Kit (ATSAME54-XPRO) | SleepWalking Application on the SAM E54 Xplained Pro Evaluation Kit. | Link |
| 31 | Automation | SAM E54 Xplained Pro Evaluation Kit (ATSAME54-XPRO) | EEPROM Temperature Logger Application on the SAM E54 Xplained Pro Evaluation Kit using FreeRTOS. | Link |
| 32 | Automation | SAM E54 Curiosity Ultra Development Board (DM320210) | Motion Surveillance Application on the SAM E54 Curiosity Ultra Development Board. | Link |
| 33 | Bootloader | SAM E54 Curiosity Ultra Development Board (DM320210) | Live Update Application on the SAM E54 Curiosity Ultra Development Board. | Link |
| 34 | Audio, Consumer | SAM E54 Curiosity Ultra Development Board (DM320210) | SD Card USB Audio Player on the SAM E54 Curiosity Ultra Development Board + maXTouch® Curiosity Pro Board using Legato Graphics. | Link |
| 35 | microSD | SAM E51 Curiosity Nano Evaluation Kit (EV76S68A) | This application showcases the capabilities of the microSD Click module. It demonstrates various file operations that can be performed on an SD card. | Link |
| 36 | 13DOF | SAM E51 Curiosity Nano Evaluation Kit (EV76S68A) | This application demonstrates the reading of weather parameters (temperature, pressure, humidity, and gas resistance) from BME680 sensor, motion parameters (gyroscope, accelerometer) in X, Y, and Z axes from BMI088 sensor,Geomagnetic data in X, Y, and Z axes from BMM150 sensor. | Link |
| 37 | Eink E-Paper display 2,9" 296 x 128 dots display | SAM E51 Curiosity Nano Evaluation Kit (EV76S68A) | This example demonstrates the display capability of E-Ink E-Paper display 2.9" 296 x 128 dots display board on the SAM E51 Curiosity Nano Evaluation Kit. | Link |
| 38 | MCP25625 | SAM E51 Curiosity Nano Evaluation Kit (EV76S68A) | This example demonstrates the transmitting and receiving of CAN data using the MCP25625 CAN click board and displays the transmit/receive CAN message on a serial terminal on the SAM E51 Curiosity Nano Evaluation Kit using the MCP25625 Click board. | Link |
| 39 | Barcode Scanner | Integrated Graphics and Touch (IGaT) Curiosity Evaluation Kit (EV14C17A) | This application detects the EAN-13 barcode and decodes it with the help of the ArduCAM Mega camera module. The ArduCAM Mega captures an image with a resolution of 1920 x 1080 and stores the image in an internal memory. The decoded barcode is then displayed on the serial console and graphical display. | Link |
| 40 | RNBD | SAM E51 Curiosity Nano Evaluation Kit (EV76S68A) | RNBD451 add-on board Example on the SAM E51 Curiosity Nano Evaluation Kit. | Link |
| 41 | DRAM | SAM E51 Curiosity Nano Evaluation Kit (EV76S68A) | DRAM Click Example on the SAM E51 Curiosity Nano Evaluation Kit. | Link |
| 42 | Flash 2 | SAM E51 Curiosity Nano Evaluation Kit (EV76S68A) | Flash 2 Click Example on the SAM E51 Curiosity Nano Evaluation Kit. | Link |
More application demonstrations are available at Microchip's MPLAB Harmony GitHub repositories. Refer to the following links:
- More application demonstrations on the SAM E51 Curiosity Nano Evaluation Kit and other Development Boards/Kits having the same part number (ATSAME51J20A)
- More application demonstrations on the SAM E54 Xplained Pro Evaluation Kit and other Development Boards/Kits having the same part number (ATSAME54P20A)
- More application demonstrations on the SAM E54 Curiosity Ultra Development Board and other Development Boards/Kits having the same part number (ATSAME54P20A)
- More application demonstrations on IGAT Kit and other Development Boards/Kits having the same part number (ATSAME51J20A)
SAM D5x/E5x Reference Designs/Solutions
| Sl. No | Type | Hardware Board/Kit Used | Description | Link |
|---|---|---|---|---|
| 1 | HMI | Integrated Graphics and Touch (IGaT) Curiosity Evaluation Kit (EV14C17A) | Low-Cost GUI With Graphics and Touchscreen Demonstration. | Link |
| 2 | HMI | Integrated Graphics and Touch (IGaT)
Curiosity Evaluation Kit (EV14C17A) or SAM E54 Curiosity Ultra Development Board (DM320210) | Graphical User Interface Demonstrations: MPLAB Harmony v3 has various demonstration examples for creating an intuitive and reliable GUI in applications. | Ref design Link and |
| 3 | Motor Control | dsPICDEM MCLV-3 Development Board
High Voltage (DM330023-3) dsPICDEM MCLV-2 Development Board Low Voltage (DM330021-2) ATSAME54 Motor Control Plug In Module (MA320207) | Motor Control for Appliances. There are multiple demonstration examples, which are pre-configured to run on Microchip’s various motor control development boards for easy prototyping of motor drive applications. | Ref Design Link and |
| 4 | Connectivity | SAM E54 Xplained Pro Evaluation Kit (ATSAME54-XPRO) | Vending Machine Demonstration: This solution demonstrates an embedded network application to update and track the status of the drinks being offered in a vending machine. | Link |
| 5 | IoT | SAM E51 Curiosity Nano Evaluation Kit (EV76S68A) | IoT Smart Appliance Control
Demonstration: This solution showcases smart control of a fan
through an Android™-based smartphone using a Bluetooth Low Energy
(BLE) connection. This solution is done for the PIC32CM MC00 Curiosity Nano. It can be ported for the SAM E51 Curiosity Nano (EV76S68A). | Link |
| 6 | IoT | SAM E51 Curiosity Nano Evaluation Kit (EV76S68A) | Fitness Tracker Wearables Demonstration: This fitness tracker demonstration displays the heart rate readings measured in beats per minute (bpm) on a low-power E-Ink display, and optionally posts this data to the Microchip Bluetooth Data mobile application for Android through Bluetooth Low-Energy technology. | Link |
| 7 | CAN, USB | SAM E54 Xplained Pro Evaluation Kit (ATSAME54-XPRO) | This reference design acts as a CAN-USB bridge along with CAN- based NVM bootloader host application. With CAN-USB bridge functionality, it reads the data transmitted on a CAN network through the CAN peripheral and displays it on the PC serial terminal window using the USB CDC virtual COM port. With CAN NVM bootloader host functionality, it sends the binary image from the Python script to the target over the CAN bus for programming. | Link |
| 8 | IoT, Consumer, Industrial, Appliance | SAM E51 Curiosity Nano Evaluation Kit (EV76S68A) | This reference application demo for an industrial environmental sensor is based on the APC-1001J (Air Quality Combo Sensor) from ScioSense, which utilizes 10BASE-T1S Ethernet communication for industrial IoT systems. This technology enables full TCP/IP integration from the sensor to the cloud, facilitating easy backend maintenance, low latency and straightforward integration and installation. The software architecture is hardware independent, offering maximum adaptability across various Microchip MCU device families and allowing users to select the best option for their sensor applications. | Link |
SAM D5x/E5x Key Links
- SAM E51 Curiosity Nano Evaluation Kit (EV76S68A)
- SAM E54 Xplained Pro Evaluation Kit (ATSAME54-XPRO)
- Integrated Graphics and Touch (IGaT) (EV14C17A)
- SAM E54 Curiosity Ultra Development Board (DM320210)
- MPLAB Harmony v3 Landing Page.
- MPLAB® Harmony v3 Reference Applications for SAM MCU
- Microchip Reference Designs Page
- 32-bit MCUs Rapid Prototyping page