The stack is accessible through the TOSH, TOSL and STKPTR registers. STKPTR is the
current value of the Stack Pointer. TOSH:TOSL register pair points to the TOP of the
stack. Both registers are read/writable. TOS is split into TOSH and TOSL due to the
15-bit size of the PC. To access the stack, adjust the value of STKPTR, which will
position TOSH:TOSL, then read/write to TOSH:TOSL. STKPTR is five bits to allow detection
of overflow and underflow.
Important: Care should be taken when modifying
the STKPTR while interrupts are enabled.
During normal program operation, CALL,
CALLW and interrupts will increment STKPTR while
RETLW, RETURN, and RETFIE will
decrement STKPTR. STKPTR can be monitored to obtain the value of stack memory left at
any given time. The STKPTR always points at the currently used place on the stack.
Therefore, a CALL or CALLW will increment the STKPTR
and then write the PC, and a return will unload the PC value from the stack and then
decrement the STKPTR.
Reference the following figures for examples of accessing the stack.Figure 9-10. Accessing the Stack Example
1Figure 9-11. Accessing the Stack Example
2Figure 9-12. Accessing the Stack Example
3Figure 9-13. Accessing the Stack Example
4
The online versions of the documents are provided as a courtesy. Verify all content and data in the device’s PDF documentation found on the device product page.