1 Harmony 3 Driver and System Service Application Examples for SAMA7D65 Family
The following applications are provided to demonstrate the typical or interesting usage
models of one or more drivers, system services and RTOS.
| Name | Description |
|---|---|
| Dynamic Voltage and Frequency Scaling (DVFS) | This MPLAB® Harmony example application demonstrates and evaluates Dynamic Voltage and Frequency Scaling (DVFS) mechanisms by simulating various CPU workloads and observing the resulting system behavior. |
| FAT Filesystem Using SDMMC Media | This application shows an example of using the MPLAB Harmony File System to access and modify the contents of a SD card using the SDMMC driver. |
| FAT Filesystem Using SST26 Media | This application shows an example of using the FAT File System to access SQI based SST26 Flash media. |
| FreeRTOS Basic | This example application demonstrates context switching between four tasks of different priorities. Two tasks run periodically while the other two tasks are event driven. |
| I2C Driver Asynchronous - I2C EEPROM | This example application shows how to use the I2C driver in Asynchronous mode to perform operations on the EEPROM. |
| I2C Driver Synchronous - I2C EEPROM | This example application shows how to use the I2C driver in Synchronous mode to perform operations on the EEPROM. |
| I2C EEPROM AT24 Driver - EEPROM Read Write | This example application shows how to use the AT24 driver to perform read and write operations on AT24 series of EEPROM. |
| SMC NAND Flash Driver - NAND Flash Read Write | This example application shows how to use the NAND Flash driver to perform read and write operations on NAND Flash device. |
| SPI Driver Asynchronous - Multi Client | This example demonstrates how to use single instance of the SPI driver in Asynchronous mode to communicate with multiple EEPROMs. |
| SPI Driver Synchronous - Multi Client | This example demonstrates how to use single instance of the SPI driver in Synchronous mode to communicate with multiple EEPROMs in an RTOS environment. |
| SPI EEPROM AT25 Driver - EEPROM Read Write | This example application shows how to use the AT25 driver to perform read and write operations on AT25 series of EEPROM. |
| Time System Service Multi-client | This example application demonstrates the multi-client system timer functionality. |
| USART Driver Asynchronous - USART Echo | This example echoes the received characters over the console using the USART driver in Asynchronous mode. |
| USART Driver Synchronous - USART Echo | This example echoes the received characters over the console using the USART driver in Synchronous mode. |