3 Using AT91Boostrap Loader With Harmony 3 MPU Applications
MPU harmony3 applications are compiled and linked to execute from external DRAM memory that is available on the corresponding evaluation kit. This require all peripherals and clock leading to the DRAM memory to be configured prior to the application being programmed into DRAM. This is achieved using a bootstrap loader. AT91bootstrap loader is used for this purpose.
The user has deployed the following pre-built bootstrap binaries inside the application repositories. They can be found under deps folder at the root of the repository.
| Binary Name | Description |
|---|---|
| at91bootstrap.elf | Bootstrap which allows debug or run application using MPLAB X |
| boot.bin | Bootstrap which allows booting application using an SD card |
To use at91boostrap to load and run harmony applications from MPLAB X, it should be build with bkptnone_defconfig configuration. If the user is interested in building at91bootstrap using MPLAB X, the user can read about it here.
Configure a Debug Tool
- Open the MPLAB X application that the user wants to debug or run in MPLAB X
- Right click the application
project and select properties. This will open the properties window. In the
Configuration option>Connected Hardware Tools, select the
debugger.
Note: If no debugger is connected, click Show All check box and select the supported debugger. - Select the target toolchain and click Apply to save the changes
- This will result in an additional
menu option to be available in the configuration tree view called Bootstrap as
shown below:

Configure a Bootstrap
- Click Use bootstrap check box to enable bootstrap support
- Click the Load button to load the bootstrap file. This will open a file picker, which allows the user to choose the bootstrap binary file.
- Navigate to the {repository
root}/deps/{board name}/at91bootstrap_binaries folder as explained in
the previous section. The user should choose at91bootstrap.elf file
(The Bootstrap entry address and the Bootstrap load address
text box can be left empty as this information will be read from the ELF file
automatically).

Run/Debug MPU Applications Using MPLAB X
The user can Run/Debug the MPU application just as any other MPLAB X applications. When executed, MPLAB X performs a two stage loading:
- Stage 1: Loads the bootstrap loader into the internal SRAM and executes it. This will configure the board specific peripherals and memory.
- Stage 2: Loads the application into the external DRAM and debugs it. User can perform actions, such as setting breakpoints, single-stepping, etc.
When using MPLAB X to debug a harmony application, the user will face the following limitations:
- Call stack is not fully supported yet, therefore stepping in and out of functions may not work correctly.
Boot to Application Using SD Card
Copy both the application binary named harmony.bin and the bootstrap binary named boot.bin onto an SD card. Insert the SD card into the SD slot of the evaluation kit and press the Reset button.
The ROM bootloader will copy the bootstrap binary boot.bin into the internal SRAM and executes it. The bootstrap will configure the external DRAM and the required peripherals, then copy the application binary harmony.bin into the DRAM and executes it.