4 Getting Started with Software Development
This section gives a detailed information on the steps to install IDE, compiler, tool chain, wireless stacks and application examples on the PC. Prior to each release, the wireless stack and application examples are thoroughly tested against a snapshot of tool versions and other software dependencies. This guide provides information on setting up the development environment with all the required dependency versions and provide detailed steps to fulfill all the dependencies.
If the user is already familiar with Microchip Tools, then the following table summarizes the dependencies.
Tools and Harmony Component Versions
Tool Chain
| Tool Chain |
Version |
Location |
|---|---|---|
|
MPLAB X IDE |
6.25 | |
|
XC32 Compiler |
4.60 | |
|
Microchip Code Configurator(MCC) |
5.6.2 | |
| Device Family Pack (DFP) |
1.3.38 | Microchip Packs Repository |
| Tool Packs | Latest provided in MPLABX | MPLABX IDE > Tools > Packs > Tool Packs |
| CMSIS Packs |
6.2.0 | Project Properties > Confg > Packs > CMSIS. For more details, refer to the Opening, Building and Programming an Existing Application Example |
Harmony Components
Use Content Manager (CM) to download the following Harmony components.
It will download the Harmony components to
C:\Users\XXX\.mcc\harmony\content.
|
Harmony Components |
Version |
|---|---|
|
csp |
v3.22.7 |
|
core |
v3.15.5 |
|
bsp | v3.22.0 |
| FreeRTOS-Kernel | V11.1.0 |
| CMSIS_5 | 5.9.0 |
|
wireless_ble | v1.5.0 |
|
wireless_pic32cxbz_wbz |
v1.6.0 |
|
wireless_system_pic32cxbz_wbz | v1.8.0 |
|
wireless_thread | v1.3.0 |
| openthread | mchp_harmony_wireless_thread_v1.3.0 |
| wireless_15_4_mac | v1.2.0 |
| wireless_15_4_phy | v1.4.0 |
| net | v3.14.2 |
| usb | v3.16.0 |
| gfx | v3.16.2 |
| Touch | v3.19.0 |
Application Example
Use Microchip Discover to download the following example code.
C:\Users\XXX.mcc\harmony\content. Therefore, users can decide on
their own folder and download the code. There are different categories of
application code. This user guide only describes wireless_apps_pic32_bz6. Users can
find the user guide of other application code when they click the link provided in
the table. | Name | Version | Applications |
|---|---|---|
| v1.1.0 | Wireless with below applications | |
| core_apps_pic32cxbz6_wmbz6(1) | v3.0.1 | Peripheral driver |
| csp_apps_pic32cxbz6_wmbz6(1) | v3.0.1 | System middleware |
| net_apps_pic32_bz6(1) | v1.0.0 | TCPIP |
| usb_apps_device(1) | v3.10.0 | USB device |
| usb_apps_host(1) | v3.10.0 | USB host |
|
Note:
| ||
Insert the above “Name” in the search field to find the example in Microchip Discover.
For more details, refer Download Application Example from Discover in Running a Precompiled Application Example from Related Links. For usb_apps_host and usb_apps_device, ensure to include “pic32wm_bz6204” in the search field.