5.7.1 Updating the Application Using a Bootloader Client With Multiple Images and Anti-Rollback Protection
This section demonstrates how to configure the application for a bootloader client with multiple image and anti-rollback protection support.
footer_certificate.c file which needs to be updated with valid
addresses depending upon the application start address and size of the execution space. Description: This section details how to update the data in the
footer_certificate.c file and configure the linker settings of the
application project for multi-image support.
-
Create a new file or open the existing
footer_certificate.cfile from the application project.Note: The application builder automatically generates this file.Figure 5-198. Open footer_certificate.cFile
-
Add the following macros at top of the file and update the image ID for the backup image according to the configuration on the MDFU client UI. For this example, the backup image ID is 3.
Note: The execution image ID will always be 0x0000.#define EXECUTION_IMAGE_ID 0x0000 #define BACKUP_IMAGE_ID 0x0003 -
Add the following code after the macro definitions.
volatile const uint16_t #ifdef __XC8__ __at(0x9AF0) #endif applicationId __attribute__((used, section("app_id"))) = EXECUTION_IMAGE_ID; volatile const uint32_t #ifdef __XC8__ __at(0x9AF2) #endif applicationVersion __attribute__((used, section("app_version"))) = 0x00000300; volatile const uint32_t #ifdef __XC8__ __at(0x9AF6) #endif verificationEndAddress __attribute__((used, section("crc_end_address"))) = 0x00009AFD; volatile const uint32_t #ifdef __XC8__ __at(0x9AFA) #endif verificationStartAddress __attribute__((used, section("crc_start_address"))) = 0x00002400;Understanding the variables stored in the footer data of the Flash memory:Table 5-3. Footer Certificate Data Variable Purpose Address applicationId This is the location where the current image will be stored. Current Example Value: EXECUTION_IMAGE_ID
Should be: Image ID of the image location to update
The address in the __at()is calculated by subtracting two from the start address of the applicationVersion.The two bytes are used for storing the uint16_t type variable applicationId.
This value might change for your application.
applicationVersion This is the version of the current application. Current Example Value: 0x00000300
Should be: Version of the application
Warning: Application version cannot be 0 or 4294967295 (0xFFFFFFFF).The address in the __at()is calculated by subtracting four from the start address of the verificationEndAddressThe four bytes are used for storing the uint32_t type variable applicationVersion.
If rollback protection is enabled, this value must be updated whenever a new application image needs to be loaded.
verificationEndAddress This is the last address that is considered for the hash calculation mapped into the execution space. The value of this argument must always fall within the execution space.
Current Example Value: 0x00009AFD
Should be: Execution Image End Address
The address in the __at()is calculated by subtracting four from the start address of the verificationStartAddressThe four bytes are used for storing the uint32_t type varible verificationEndAddress.
This value might change for your application.
verificationStartAddress This is the first address that is considered for the hash calculation mapped into the execution space. The value of this argument must always fall within the execution space.
Current Example Value: 0x00002400
Should be: Execution Image Start Address
The address in the __at()is calculated by subtracting six from the end address of the application image to be verified.The six bytes are the sum of the two bytes for storing the checksum and four bytes for storing the uint32_t type variable verificationStartAddress.
Tip: Populate the addresses following a bottom-up approach for easier calculations.This value might change for your application.
- Add the following code in the
footer_certificate.cfile after the macros. This reserves the last bytes to hold the Checksum value. The address presented below in the__at()is the execution image end address - 2, since the Checksum hash size used is two bytes and we are locating the end of the application to be the execution space. This address may be different for your device.volatile const uint16_t #ifdef __XC8__ __at(0x9AFE) #endif checksumStart __attribute__((used, section("checksum_data"))) = 0xFFFF;Tip: For more information on how to define this variable, refer to point 9 from Creating an Application for PIC® Devices. - Additionally, linker settings need to
be updated to restrict the ROM range to the current application image ID’s Flash
range.
- For PIC devices:
Figure 5-199. Compiler - Linker Settings 
Where 2400-9AFF is
<applicationId image start address: applicationId image end address>. These values can be updated by referring to the Device Flash Memory Partitions Table in the MDFU Client UI and the applicationId. - For AVR devices:
For an AVR-based bootloader client with applicationid image range of 0x2400-0x9AFF the linker settings are as follows:
- XC8 linker
settings:Open Project Properties>XC8 Linker>Additional Options. In the “Additional Options” text box, add
-Wl,-u,checksumStart,-u,verificationStartAddress,-u,verificationEndAddress,-u,applicationVersion,-u,applicationId,-u,__TEXT_REGION_LENGTH__=<applicationId image start address: applicationId image end address>,-Ttext=<applicationId image start>Figure 5-200. XC8 Linker Settings 
- GCC linker
settings:Open Project Properties>Avr GCC (Global Options)>avr-ld>General. In the “Additional Options” text box, add
-Wl,-u,checksumStart,-u,verificationStartAddress,-u,verificationEndAddress,-u,applicationVersion,-u,applicationId,-u,__TEXT_REGION_LENGTH__=<applicationId image start address: applicationId image end address>,-Ttext=<applicationId image start>Figure 5-201. GCC Linker Settings 
- XC8 linker
settings:
- For PIC devices: