4.3.5 MAC Address Programming

In this demonstration, the user can set the Bluetooth address and 802.15.4 MAC address of the PIC32-BZ6 using a PC with the MCHPRT3 tool installed.

In the MAC Address tab, perform the following steps for MAC Address programming:
  1. From the IB Type drop-down list, select Flash (default value).
  2. To read the Bluetooth address from the IB, click Read BT Addr from IB.
  3. To write the Bluetooth address:
    1. Click Write BT Addr to IB Buffer.
    2. Click Commit BT Addr IB Buffer to IB.
  4. To read the 802.15.4 MAC address from IB, click Read 802.15.4 Addr from IB.
  5. To write 802.15.4 MC address:
    1. Click Write 802.15.4 Addr to IB Buffer.
    2. Click Commit 802.15.4 Addr IB Buffer to IB.
Figure 4-18. MCHPRT3 PIC32-BZ6 GUI for MAC Address Programming