4.3.1 Using a Graphical SCP Utility
(Ask a Question)To transfer files to the kit, perform the following steps:
-
Launch the transfer manager of your choice (in this case, WinSCP is used) and connect to the kit. In this case, the SCP protocol is used.
Figure 4-5. Launch Transfer Manager
Once connected, you have the access to the home folder of the ubuntu user (that is, /home/ubuntu) – files can be transferred to any directory.
- Drag the file to the desired
directory—verify the transfer using the
lscommand.Figure 4-6. Transfer File - SCP commands can also be run from
terminal/command line, for
example:
scp .\Microchip_logo.svg.png ubuntu@10.145.200.55:/home/ubuntu/test