3.2 Labels
The PIC Assembler is more strict than MPASM regarding the definition of labels.
A label is a symbolic alias that is assigned a value equal to the current location within the current psect. This assignment is typically performed by the linker.
In the PIC Assembler, a label definition consists of any valid assembly
identifier followed by a colon, :. In MPASM, the colon is option. When
migrating, you must add colons to any label in MPASM code that does not already use
one.
Label identifiers used by the PIC Assembler are always case sensitive.
A label identifier can contain any number of characters drawn from the
alphabetics, numerics, and the special characters: dollar, $; question
mark, ?; and underscore, _. The first character of an
identifier cannot be numeric. A identifier cannot have the same name as any of the
assembler directives, keywords, or psect flags. A label definition can appear on a line
by itself or it can be positioned to the left of an instruction or assembler
directive.
The following shows the definition of valid and unique labels in the PIC Assembler.
An_identifier:
movlw 55
an_identifier: movlw 0AAh
an_identifier1: DW 0x1234
?$_12345:
return