5.2 Placing Psects into Memory
All code and objects must be placed in a psect (program section). This groups together similar parts of a program and allows you to link those sections using the psect’s name. All psects are allocated memory by the linker, after which, the values for any labels defined in those psects can be determined.
- If the psect specifies the
absflag, it is placed at address 0 in the memory space indicated by the psect'sspaceflag, or the program memory (default) space if no space has been specified. - If a
-plinker option references the psect name, the psect is placed at the location specified by that option in the memory space indicated by the psect'sspaceflag, or the program memory (default) space if no space has been specified. - If the psect is associated with a linker class, the psect is placed at any free location in the address ranges defined by that class.
- If the psect specifies a space number, it is placed at a free location in that memory space (Not recommended).
- The psect is placed in a free location in the program memory (default) space (Not recommended).
Some situations are illegal, for example if you use a -p
option to place a psect that also uses the abs flag, then an error will
be issued. It is recommended that psects are always linked using the
abs flag, using a -p option, or via a linker class
(the first three of the above methods). If the linker has to position a psect with no
guidance from the user (the last two of the above methods), a warning similar
to,(526) psect "wanderer" not specified in -P option (first appears in
"not_right.o"), will be emitted.
PSECT udata_bank1
myVar:
DS 2the
udata psect has already been associated with the
RAM linker class and will be linked anywhere in free memory
associated with that class.class flag with the psect definition. In the following example, a
psect has been created by the programmer to use instead of
udata.PSECT machData,space=1,class=MDATA
myVar:
DS 2This
psect uses a new class, MDATA, which will need to be defined by a
linker option. To do that, use, for example, the driver option,
-Wl,-AMDATA=050h-05fh, which passes the -A linker
option directly to the linker and which will associate the specified address range with
the MDATA class.There are, however, times when a psect must be placed at a specific address.
The reset vector code is one good example, as are interrupt routines. In this case, you
will need to use a -p linker option to place the psect at the desired
location. This might be as simple as providing an absolute address, for example using
the driver option -Wl,-pInterrupt=08h to place the psect called
Interrupt at address 8, but there are more advanced usages of this
option.
Check the MPLAB® XC8 PIC Assembler User's Guide for full details concerning the psects and linker classes provided by the PIC Assembler, as well as the linker and driver options mentioned in this section.