1.11 FILEX Filesystem using SST26 Media
This application shows an example of using the FILEX File System to access SQI based SST26 flash media.
Description
File System Operations on the On-Board SST26 Flash Memory:
- Performs a SYS_FS_FormatDisk
 - Opens a newfile.txt on the SST26 flash
 - Write and reads back 4KB of data on newfile.txt
 - Verifies the Data Read back
 
File system layer uses:
- One instance of the Memory driver is used to communicate with the On-Board SQI Flash memory
 
Downloading and Building the Application
To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.
Path of the application within the repository is apps/fs/sqi_flash_filex/firmware.
To build the application, refer to the following table and open the project using its IDE.
| Project Name | Description | 
|---|---|
| sam_e54_xpro.X | MPLABX project for SAM E54 Xplained Pro Evaluation Kit | 
Setting Up the Hardware
The following table shows the target hardware for the application projects.
| Project Name | Description | 
|---|---|
| sam_e54_xpro.X | SAM E54 Xplained Pro Evaluation Kit | 
Setting Up SAM E54 Xplained Pro Evaluation Kit
- Connect the Debug USB port on the board to the computer using a micro USB cable
 
Running the Application
- Build and program the application using its IDE
 - The LED is turned ON if data has successfully been written and read back from file “newfile.txt”
 
Refer to the following table for LED name:
| Board | LED Name | 
|---|---|
| SAM E54 Xplained Pro Evaluation Kit | LED0 |