1.3 FAT File System using NVM and SD Card Media
This application shows an example of using the FAT File System to access files across multiple media (NVM, SD Card).
Description
File System Operations on NVM and SD Card:
- The application contains a FAT disk image consisting of a Master Boot Record (MBR) sector, Logical Boot Sector, File Allocation Table, and Root Directory Area, placed in the internal Flash memory (NVM)
 - A SD card is used as another disk, which might have FAT16 or FAT32 implemented on it (dependent on the formatting of SD card)
 - The application searches the NVM media for a named FILE.TXT, opens and reads the contents of the file in NVM and copies the contents to the file, FILE.TXT, in the SD card
 - Once the copy is successful, an addition string “Test is successful” is added to the file. If the write operation is successful, LED indication is provided
 
File system layer uses:
- Memory driver to communicate with underlying NVM media
 - SDSPI Driver to communicate to SD Card over SPI
 
Downloading and Building the Application
To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.
Path of the application within the repository is apps/fs/nvm_sdspi_fat_multi_disk/firmware.
To build the application, refer to the following table and open the project using its IDE.
| Project Name | Description | 
|---|---|
| sam_e54_xpro_freertos.X | MPLABX project for SAM E54 Xplained Pro Evaluation Kit | 
Setting Up the Hardware
The following table shows the target hardware for the application projects.
| Project Name | Description | 
|---|---|
| sam_e54_xpro_freertos.X | SAM E54 Xplained Pro Evaluation Kit | 
Setting Up SAM E54 Xplained Pro Evaluation Kit
- To run this demo, following additional hardware is required:
- I/O1 Xplained Pro Extension Kit
 - micro-SD card formatted to FAT filesystem
 
 - Connect I/O1 Xplained Pro Extension Kit to the EXT1 connector
 - Insert the micro-SD Card in the micro-SD Card slot of the I/O1 Xplained Pro Extension Kit
 - Connect the Debug USB port on the board to the computer using a micro USB cable
 
Running the Application
- Build and program the application using its IDE
 - The LED is turned ON when the content from the NVM media is copied to SD-Card
                        successfullyRefer to the following table for LED name:
Board LED Name SAM E54 Xplained Pro Evaluation Kit LED0  - If Success, Insert the SD Card on to your host PC
 - FILE.txt should have the content “This data from NVM Disk Test is successful”