1.1.3 SAM E70 Xplained Ultra Evaluation Kit: Building and Running the SDCARD Bootloader applications
Downloading and building the application
To clone or download this application from Github,go to the main page of this repository and then click Clone button to clone this repo or download as zip file. This content can also be download using content manager by following these instructions
Path of the application within the repository is apps/sdcard_bootloader/
To build the application, refer to the following table and open the project using its IDE.
Bootloader Application
| Project Name | Description |
|---|---|
| bootloader/firmware/sam_e70_xult.X | MPLABX Project for SAM E70 Xplained Ultra Evaluation Kit |
Test Application
| Project Name | Description |
|---|---|
| test_app/firmware/sam_e70_xult.X | MPLABX Project for SAM E70 Xplained Ultra Evaluation Kit |
Setting up SAM E70 Xplained Ultra Evaluation Kit
- Connect the Debug USB port on the board to the computer using a micro USB cable
- Use the micro sdcard slot at the bottom of the device to insert a micro sdcard
Running the Application
Open the test application project test_app/firmware/sam_e70_xult.X in the IDE
Build the project to generate the binary (Do not program the binary)
Open the bootloader project bootloader/firmware/sam_e70_xult.X in the IDE
Build and program the application using the IDE
LED1 will be Turned On once programming is completed and bootloader starts running
Open the Terminal application (Ex.:Tera Term) on the computer to get test application messages through UART once bootloaded
Configure the serial port settings as follows:
- Baud : 115200
- Data : 8 Bits
- Parity : None
- Stop : 1 Bit
- Flow Control : None
Copy the generated application binary file to a micro sdcard from the Host PC
- <harmony3_path>/bootloader_apps_sdcard/apps/sdcard_bootloader/test_app/firmware/sam_e70_xult.X/dist/sam_e70_xult/production/sam_e70_xult.X.production.bin
Rename the copied application binary file to image.bin
Insert the micro sdcard with the application binary image.bin to the micro sdcard slot on the device
Once the application is successfully programmed LED1 should start blinking and you should see below output on the console

Remove the micro sdcard from the sdcard slot
Press and hold the Switch SW0 to trigger Bootloader from test application and you should see below output

Repeat Steps 10-12 once and jump to Step-15
- This step is to verify that bootloader is running after triggering bootloader from test application in Step 13
Press and hold the Switch SW0 and then press Reset button or Power cycle the device to force trigger bootloader at startup
Repeat Steps 10-12 once
- This step is to verify whether bootloader is triggered by switch press at reset
Additional Steps (Optional)
To bootload any other application refer to Application Configurations
Once done repeat the applicable steps mentioned in Running The Application