1.1 SDCARD Bootloader
This example application shows how to use the File System Bootloader Library to bootload an application using SDCARD protocol.
Bootloader Application
- This is a bootloader application which resides from
- The starting location of the flash memory region for SAM devices
- The starting location of the Boot flash memory region for PIC32MZ devices
- The starting location of Program Flash memory for PIC32MK and PIC32MX devices
- It uses the Harmony 3 File System Framework to receive the application binary from a sdcard
- It calls the bootloader_Tasks() function which receives application to be programmed into flash memory from a sdcard
- It glows an LED once bootloader firmware is running
- Trigger Methods
- It uses the On board Switch as bootloader trigger pin to force enter the bootloader at reset of device
- It checks for bootloader request pattern (0x5048434D) from the starting 16 Bytes of RAM to force enter bootloader at reset of device
Test Application
- This is a test application which resides from
- The end of bootloader size in device flash memory for SAM devices
- The end of bootloader size in Program Flash memory for PIC32MK and PIC32MX devices
- The start of Program Flash memory for PIC32MZ devices
- It will be loaded into flash memory by bootloader application
- It blinks an LED and provides console output
- It uses the On board Switch to trigger the bootloader from firmware
- Once the switch is pressed it loads first 16 bytes of RAM with bootloader request pattern (0x5048434D) and resets the device
Development Kits The following table provides links to documentation on how to build and run SDCARD bootloader on different development kits