2.2 Card Detect on SDMMC not functional
The Card Detect feature in the SDMMC memory interface in the Boot Configuration Packet is not functional.
If an SDMMC interface is selected as the boot media, the Card Detect pin the user may have indicated in the options is not taken into account. The ROM code looks for a valid bootstrap even if the Card Detect pin is high (no card inserted).
Work Around
None
Affected Device Revisions
| A1 | A2 | ||||||
| X | X |