36.3.7 Bus Time-Out
The SMBus protocol requires a bus watchdog to prevent a stalled device from holding the bus indefinitely. The I2C Bus Time-Out Clock Source Selection (I2CxBTOC) register provides several clock sources that can be used as the time-out time base. The I2C Bus Time-Out (I2CxBTO) register is used to determine the actual bus time-out time period, as well as how the module responds to a time-out.
- SCL =
0
(regardless of whether or not the bus is Active) - SCL =
1
and SDA =0
while the bus is Active
If either of these conditions are true, an internal time-out counter increments and
continues to increment as long as the condition stays true or until the time-out period
has expired. If these conditions change (e.g. SCL = 1
), the internal
time-out counter is reset by module hardware.
The Bus Time-Out Clock Source Selection (BTOC) bits select the time-out clock source. If an oscillator is selected as the time-out clock source, such as the LFINTOSC, the time-out clock base period is approximately 1 ms. If a timer is selected as the time-out clock source, the timer can be configured to produce a variety of time periods.
35
’ is written into the TOTIME bits, and the LFINTOSC is selected
as the time-out clock source, the time-out period is approximately 35 ms (35 x 1 ms). If
the TOBY32 bit is set (TOBY32 = 1
), the time-out period determined by
the TOTIME bits is multiplied by 32. If TOBY32 is clear (TOBY32 = 0
),
the time-out period determined by the TOTIME bits is used as the time-out period.The examples below illustrate possible time-out configurations.
35 ms BTO Period Configuration
void Init_BTO_35(void) // Selections produce a 35 ms BTO period { I2C1BTOC = 0x06; // LFINTOSC as BTO clock source I2C1BTObits.TOREC = 1; // Reset I2C interface, set BTOIF I2C1BTObits.TOBY32 = 0; // BTO time = TOTIME * TBTOCLK I2C1BTObits.TOTIME = 0x23; // TOTIME = TBTOCLK * 35 // = 1 ms * 35 = 35 ms }
64 ms BTO Configuration
void Init_BTO_64(void) // Selections produce a 64 ms BTO period { I2C1BTOC = 0x06; // LFINTOSC as BTO clock source I2C1BTObits.TOREC = 1; // Reset I2C interface, set BTOIF I2C1BTObits.TOBY32 = 1; // BTO time = TOTIME * TBTOCLK * 32 // = 2 ms * 32 = 64 ms I2C1BTObits.TOTIME = 0x02; // TOTIME = TBTOCLK * 2 // = 1 ms * 2 = 2 ms }
1
), the
I2C module is reset and module hardware sets the Bus Time-Out Interrupt Flag (BTOIF). If the Bus Time-Out Interrupt Enable (BTOIE) is also set, an interrupt will be generated. If a bus time-out occurs
and TOREC is clear (TOREC = 0
), the BTOIF bit is set, but the module is
not reset.1
) and a bus time-out event occurs
(regardless of the state of the Client Mode Active (SMA)
bit), the module is immediately reset, the SMA and Client Clock Stretching (CSTR) bits are cleared, and the Bus Time-Out Interrupt Flag (BTOIF) bit is set.0
) and a bus time-out event occurs
(regardless of the state of the Client Mode Active (SMA)
bit), the BTOIF bit is set, but user software must reset the module.1
) and the bus time-out event occurs
while the Host is active (Host Mode Active (MMA) =
1
), the Host Data Ready (MDR)
bit is cleared, the module will immediately attempt to transmit a Stop condition and the
BTOIF bit is set. Stop condition generation may be delayed if a client
device is stretching the clock, but will resume once the clock is released or if the
client holding the bus also has a time-out event occur. The MMA bit is only cleared
after the Stop condition has been generated.0
) and the bus time-out event occurs
while the Host is active (Host Mode Active (MMA) =
1
), the MDR bit
is cleared and the BTOIF bit is set, but user software must initiate the Stop condition by
setting the P
bit.The figure below shows an example of a Bus Time-Out event when the module is operating in Host mode.