2.5.1 Windows
When installing the JTAGICE mkII on a computer running Microsoft® Windows®, the USB driver is loaded when the unit is first powered up.
Note: Be sure to install the
front-end software packages before powering up for the first time.

Proceed with the default ("recommended") options through the New Hardware Wizard.


If it is not detected automatically, point the wizard to the device driver (provided by Jungo) called JTAGICEmkII.inf which is stored in the <windows_root>\inf folder.
Once successfully installed, the JTAGICE mkII will appear in the device manager as a "Jungo" device.

Your JTAGICE mkII is now ready to use.