1.7.1 How the UDP Bootloader library works

The UDP Bootloader firmware communicates with the Unified Host application running on Host PC by using a predefined communication protocol.

The UDP Bootloader works in two different modes

Basic Mode

  • This mode is supported for all the devices

  • Resides from

    • The starting location of the flash memory region for CORTEX-M based MCUs

    • The starting location of the Boot flash memory region or Program flash memory region for MIPS based MCUs devices

  • The Bootloader performs flash erase/program/verify operations with the application hex sent from host PC using the Unified Bootloader Host Application while in the firmware upgrade mode

    • Bootloader always performs flash operation from the address received via hex record

    • The application can use the entire flash memory region starting from the end of bootloader space

  • Jumps to the application once programming is completed

Live Update Mode

  • This mode is supported for the devices which have a Dual Bank flash memory

  • Resides from

    • The starting location of the flash memory region of both the banks on CORTEX-M based MCUs along with application code

    • The starting location of the Program flash memory region of both the banks for MIPS based MCUs devices along with application code

  • The Bootloader task performs flash erase/program/verify operations with the application hex sent from host PC using the Unified Bootloader Host Application in the Inactive bank

  • Performs a bank swap and reset to run the application programmed in inactive bank on application task request