2.4.2 Subscribing to AWS Shadow Topic
To get information about the device’s shadow from the shadow service, the device has to subscribe to specific shadow topics. More information on shadow topics can be found here at Shadow MQTT topics.
The device subscribes to
‘$aws/things/thingName/shadow/update/delta’.The shadow service will
send updates on this topic when there is a difference in attribute values. For example,
the reported toggle state is 1 but a client sent a desired state for toggle as 0. The
device would receive update like below:
{
"version": 1349,
"timestamp": 1583450271,
"state": {
"toggle": 0
},
"metadata": {
"toggle": {
"timestamp": 1583450271
}
}
}
Further information can be found here: /update/delta