Jump to main content
         
        
        
        
        
        
        
        
         
        
        
        
        
            
            
            
            
            
            
                
                    
                        
                            
                         
                    
                    
                    
                        
                            
                                      
                             
                         
                        
                        
                        
   24.4.1.9 Synchronous Host Reception Setup 
   
      
         Initialize the SPxBRGH:SPxBRGL 
            register pair and set or clear the BRG16  bit, as required, to achieve the desired baud rate. 
         Select the receive input pin by writing
            the appropriate values to the RxyPPS and RXxPPS registers. Both selections may enable
            the same pin. 
         Select the clock output pin by writing
            the appropriate values to the RxyPPS and TXxPPS registers. Both selections may enable
            the same pin. 
         Clear the ANSEL bit for the RXx pin (if applicable). 
         Enable the synchronous host serial port by setting the SYNC , SPEN  and CSRC  bits. 
         Ensure that the CREN  and SREN  bits are cleared. 
         If interrupts are desired, set the RCxIE bit of the PIEx
            register and the GIE and PEIE bits of the INTCON register. 
         If 9-bit reception is desired, set the RX9 
            bit. 
         Start reception by setting the SREN bit, or for continuous
            reception set the CREN bit. 
         The RCxIF Interrupt Flag bit will be set when reception of a
            character is complete. An interrupt will be generated if the RCxIE enable bit was
            set. 
         Read the RCxSTA  register to get the ninth bit (if enabled) and determine
            if any error occurred during reception. 
         Read the 8-bit received data by reading the RCxREG 
            register. 
         If an overrun error occurs, clear the error by either clearing
            the CREN bit or by clearing the SPEN bit which resets the EUSART. 
       
      Figure 24-11. Synchronous Reception (Host Mode,
            SREN)   
         
          
       
    
  
                        
                        
                        
                        
                        
                        
                     
                    
                 
             
            
            
            
          
        The online versions of the documents are provided as a courtesy. Verify all content and data in the device’s PDF documentation found on the device product page.