4.1 Example
The application note provides a code example about how to wake up ATmega328PB from the Power-down mode (which has the
least consumption of all the sleep modes) by using USART. For other sleep modes, just
change the argument in the
set_sleep_mode() function. The source code
is available for download from Atmel
START. Here below is the main()
function:int main(void)
{
power_reduction();
uart_init();
sei();
while(1)
{
if(!ring_buffer_is_empty(&ring_buffer_in)){
usart_transmit( ring_buffer_get(&ring_buffer_in));
} else {
set_sleep_mode(SLEEP_MODE_PWR_DOWN);
sleep_mode();
}
}
}