3.3 Running the Example Connect the keypad to the ATmega1627 Curiosity Nano as follows: Row 0: PB0 Row 1: PB1 Row 2: PA2 Row 3: PA1 Column 0: PC3 Column 1: PC0 Column 2: PC1 Column 3: PC2 Connect the red LED to PB3 and the green LED to PB2 Connect the ATtiny1627 Curiosity Nano to a computer using a USB cable Download the application as explained in Section Get Code Examples from Atmel START and program it to the ATtiny1627 Curiosity Nano The pin code “123ABC” is programmed to be the passcode. Try pressing this code followed by pound (#) to observe the green LED flashing. Try a different code to observe the red LED flashing.