6.4 How to Use the Hardware Tool Emergency Boot Firmware Recovery Utility

Attention: Only use this utility to restore hardware tool boot firmware to its factory state. Use only if your hardware tool no longer functions on any machine.

The debugger may need to be forced into recovery boot mode (reprogrammed) in rare situations; for example, if any of the following occurs when the debugger is connected to the computer:

  • If the debugger has no LEDs lit.
  • If the LEDs are cyan in color.
  • If the procedure described in How to Invoke the Bootload Mode was not successful.
Important: YOU MUST USE MPLAB X IDE v6.00 OR GREATER TO USE THE EMERGENCY RECOVERY UTILITY FOR MPLAB ICE 4.

Carefully follow the instructions found in MPLAB X IDE under the main menu options Debug>Hardware Tool Emergency Boot Firmware Recovery.

Figure 6-2. Selecting Emergency Utility

If the procedure was successful, the recovery wizard displays a success screen. The MPLAB ICE 4 will now be operational and able to communicate with the MPLAB X IDE. If the procedure failed, try it again. If it fails a second time, contact Microchip Support at support.microchip.com.