1 Harmony 3 Driver and System Service Application Examples for PIC32CZ CA70 Family
The following applications are provided to demonstrate the typical or interesting usage
models of one or more drivers, system services and RTOS.
| Name | Description |
|---|---|
| Console Debug System Service using UART | This example application demonstrates the UART based console and debug system service |
| EEPROM Emulator Library Read Write | This application example demonstrates how to read and write to the Emulated EEPROM memory space using the EEPROM Emulator library |
| FAT File System using NVM and SDMMC Media | This application shows an example of using the FAT File System to access files across multiple media (NVM, SDMMC) |
| FAT File System using NVM and SDSPI Media | This application shows an example of using the FAT File System to access files across multiple media (NVM, SDSPI) |
| FAT Filesystem throughput using SDMMC Media | This application calculates throughput by Writing and Reading data into a SD-Card at High Speed using the MPLAB Harmony File System and the SDMMC driver |
| FAT Filesystem using NVM and SST26 Media | This application shows an example of using the FAT File System to access multiple files across multiple media (NVM, SQI FLASH) |
| FAT Filesystem using NVM Media | This application shows an example of implementing a FAT disk in the device internal Flash memory |
| FAT Filesystem using RAM Media | This application shows an example of using the FAT File System to access RAM media |
| FAT Filesystem using SDMMC Media | This application shows an example of using the FAT File System to access and modify the contents of a SD card using the SDMMC driver |
| FAT Filesystem using SDSPI Media | This application shows an example of using the FAT File System to access and modify the contents of a SD card using the SDSPI driver and the SPI PLIB |
| FAT Filesystem using SST26 Media | This application shows an example of using the FAT File System to access SQI based SST26 flash media |
| FreeRTOS Basic | This example application demonstrates context switching between four tasks of different priorities. Two tasks run periodically while the other two tasks are event driven |
| FreeRTOS Task Notification | This example application is to illustrate the FreeRTOS Task Notification feature which is used as a light weight binary semaphore |
| FreeRTOS Tickless Basic | This example application blinks an LED to show the FreeRTOS threads that are running and to indicate status in the FreeRTOS tickless idle mode |
| I2C Driver Asynchronous - I2C EEPROM | This example application shows how to use the I2C driver in asynchronous mode to perform operations on the EEPROM |
| I2C Driver Asynchronous - Multi Client | This example application demonstrates the multi-client feature of the asynchronous mode of the I2C driver by communicating with an external EEPROM and a temperature sensor |
| I2C Driver Synchronous - I2C EEPROM | This example application shows how to use the I2C driver in synchronous mode to perform operations on the EEPROM |
| I2C Driver Synchronous - Multi Client | This example application demonstrates the multi-client feature of the synchronous mode of the I2C driver by communicating with an external EEPROM and a temperature sensor |
| I2C EEPROM AT24 Driver - EEPROM Read Write | This example application shows how to use the AT24 driver to perform read and write operations on AT24 series of EEPROM |
| Memory Driver Asynchronous - NVM SST26 Read Write | This example application shows how to use the Memory driver in asynchronous mode to perform block operations on the NVM and the SST26 media’s |
| Memory Driver Synchronous - NVM SST26 Read Write | This example application shows how to use the Memory driver in synchronous mode to perform block operations on the NVM and the SST26 media’s |
| MPFS Filesystem using NVM Media | This application shows an example of implementing a MPFS disk in device Internal Flash memory |
| SDMMC Driver Asynchronous - SDMMC Read Write | This example application shows how to use the SDMMC driver in asynchronous mode to perform block operations on the SD Card Media |
| SDSPI Driver Synchronous - SDSPI Read Write | This example application shows how to use the SDSPI driver in synchronous mode to perform block operations on the SD Card Media |
| SPI Driver Asynchronous - Multi Client | This example demonstrates how to use single instance of the SPI driver in asynchronous mode to communicate with multiple EEPROMs |
| SPI Driver Asynchronous - Self Loopback Multi Client | This example demonstrates how to use the SPI driver in asynchronous mode to achieve self-loop back between multiple clients |
| SPI Driver Synchronous - Multi Client | This example demonstrates how to use single instance of the SPI driver in synchronous mode to communicate with multiple EEPROMs |
| SPI Driver Synchronous - Self Loopback Multi Client | This example demonstrates how to use the SPI driver in synchronous mode to achieve self-loop back between multiple clients in RTOS environment |
| SPI EEPROM AT25 Driver - EEPROM Read Write | This example application shows how to use the AT25 driver to perform read and write operations on AT25 series of EEPROM |
| SST26 SQI Flash Driver - Flash Read Write in Quad IO Mode | This example application shows how to use the SST26 SQI flash driver to perform block operations on the On-Board SST26 Flash memory in Quad IO mode |
| SST26 SQI Flash Driver - Flash Read Write in SPI Mode | This example application shows how to use the SST26 driver to perform block operations on the On-Board SST26 Flash memory in SPI mode |
| Time System Service Multi-client | This example application demonstrates the multi-client system timer functionality |
| Time System Service Multi-client | This example echoes the received characters over the console using the USART driver in asynchronous mode |
| USART Driver Asynchronous - USART Multi Instance | This example echoes the received characters over the two consoles using the USART driver in asynchronous mode |
| USART Driver Synchronous - USART Echo | This example echoes the received characters over the console using the USART driver in synchronous mode |
| USART Driver Synchronous - USART Multi Instance | This example echoes the received characters over the two consoles using the USART driver in synchronous mode |