1.32 Time System Service Multi-client
This example application demonstrates the multi-client system timer functionality.
Description
- This application demonstrates timer functionality (with two clients to the Time System Service) by periodically printing a message on console every two seconds and blinking an LED every one second
- Delay, counter and single shot timer functionality is demonstrated on a switch press
- On a switch press, the application reads the current value of the 64 bit counter (say, count 1)
- It then starts a delay of 500 milliseconds and waits for the delay to expire
- Once the delay has expired, the application again reads the current value of the 64 bit counter (say, count 2) and calculates the difference between the two counter values
- The difference count indicates the time spent for the delay and is printed on the console as, “Delay time = x ms”, where x is the delay value and is equal to 500 milliseconds in the given example
- The application then starts a single shot timer of 100 milliseconds
- When the single shot timer expires, a message is printed on the console that says “Single shot timer of 100 ms expired”
- This message is printed only once on every switch press
Downloading and Building the Application
To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.
Path of the application within the repository is apps/system/time/sys_time_multiclient/firmware.
To build the application, refer to the following table and open the project using its IDE.
| Project Name | Description |
|---|---|
| pic32cz_ca70_curiosity_ultra.X | MPLABX project for PIC32CZ CA70 Curiosity Ultra Development Kit |
| pic32cz_ca70_curiosity_ultra_freertos.X | MPLABX project for PIC32CZ CA70 Curiosity Ultra Development Kit |
Setting Up the Hardware
The following table shows the target hardware for the application projects.
| Project Name | Description |
|---|---|
| pic32cz_ca70_curiosity_ultra.X pic32cz_ca70_curiosity_ultra_freertos.X | MPLABX project for PIC32CZ CA70 Curiosity Ultra Development Kit |
Setting Up PIC32CZ CA70 Curiosity Ultra Development Kit
- Connect the Debug USB port on the board to the computer using a micro USB cable
Running the Application
- Open the Terminal application (Ex.:Tera term) on the computer
- Connect to the EDBG Virtual COM port and configure the serial settings as
follows:
- Baud : 115200
- Data : 8 Bits
- Parity : None
- Stop : 1 Bit
- Flow Control : None
- Build and Program the application using its IDE
- Observe the following message getting printed on the console every two
seconds

- Press the switch and observe the following output on the terminal (highlighted
in red box)

- “Delay time = 500 ms” indicates the amount of time spent during the delay
- “Single shot timer of 100 ms expired” is printed only once on every switch press
- LED indicates the periodic timer functionality
- LED is toggled periodically every two second
Refer to the following table for Switch and LED names:
| Board | LED Name |
|---|---|
| PIC32CZ CA70 Curiosity Ultra Development Kit | LED1 |