1.16 SQI Flash SST26 Driver - SST26 SQI Read Write
This example application shows how to use the SST26 driver to perform block operations on the On-Board SST26 Flash memory in Quad IO mode.
Description
- Uses the SST26 driver to Erase/Write/Read on the On-Board SST26 Flash memory using the SQI peripheral library in Quad IO mode
- Consists of APP_SST26_Tasks() which is called through SYS_Tasks() routine
Downloading and Building the Application
To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.
Path of the application within the repository is apps/driver/sqi_flash/sst26/sst26_sqi_read_write/firmware.
To build the application, refer to the following table and open the project using its IDE.
Project Name | Description |
---|---|
pic32mz_ef_sk.X | MPLABX project for PIC32MZ Embedded Connectivity with FPU (EF) Starter Kit |
Setting Up the Hardware
The following table shows the target hardware for the application projects.
Project Name | Description |
---|---|
pic32mz_ef_sk.X | PIC32MZ Embedded Connectivity with FPU (EF) Starter Kit |
Setting Up PIC32MZ Embedded Connectivity with FPU (EF) Starter Kit
- Connect the Debug USB port on the board to the computer using a mini USB cable
Running the Application
- Build and program the application using its IDE
- The LED is turned ON when the data read from SST26 flash matches with the data written in it
Refer to the following table for LED name:
Board | LED Name |
---|---|
PIC32MZ Embedded Connectivity with FPU (EF) Starter Kit | LED3 |