1 Harmony 3 Driver and System Service Application Examples for PIC32MZ EF Family

The following applications are provided to demonstrate the typical or interesting usage models of one or more drivers and system services.

NameDescription
Console Debug System Service using UARTThis example application demonstrates the UART based console and debug system service
Console Debug System Service using USBThis example application demonstrates the USB based console and debug system service
FAT Filesystem using NVM and SDSPI MediaThis application shows an example of using the MPLAB Harmony File System to access files across multiple media (NVM, SDSPI)
FAT Filesystem using NVM and SST26 MediaThis application shows an example of using the MPLAB Harmony File System to access multiple files across multiple media (NVM, SQI FLASH)
FAT Filesystem using NVM MediaThis application shows an example of implementing a FAT disk in the device internal Flash memory
FAT Filesystem using SDSPI MediaThis application shows an example of using the MPLAB Harmony File System to access and modify the contents of a SD card using the SDSPI driver and the SPI PLIB
FAT Filesystem using SST26 MediaThis application shows an example of using the MPLAB Harmony File System to access SQI based SST26 flash media
FreeRTOS BasicThis example application demonstrates context switching between four tasks of different priorities. Two tasks run periodically while the other two tasks are event driven
FreeRTOS Task NotificationThis example application is to illustrate the FreeRTOS Task Notification feature which is used as a light weight binary semaphore
Memory Driver Asynchronous - NVM SST26 Read WriteThis example application shows how to use the Memory driver in asynchronous mode to perform block operations on the NVM and the SST26 media’s
Memory Driver Synchronous - NVM SST26 Read WriteThis example application shows how to use the Memory driver in synchronous mode to perform block operations on the NVM and the SST26 media’s.
MPFS Filesystem using NVM MediaThis application shows an example of implementing a MPFS disk in device Internal Flash memory
SDSPI Driver Synchronous - SDSPI Read WriteThis example application shows how to use the SDSPI driver in synchronous mode to perform block operations on the SD Card Media
SPI Driver Asynchronous - Self Loopback Multi ClientThis example demonstrates how to use the SPI driver in asynchronous mode to achieve self-loop back between multiple clients
SPI Driver Synchronous - Self Loopback Multi ClientThis example demonstrates how to use the SPI driver in synchronous mode to achieve self-loop back between multiple clients in RTOS environment
SQI Flash SST26 Driver - SST26 SQI Read WriteThis example application shows how to use the SST26 driver to perform block operations on the On-Board SST26 Flash memory in Quad IO mode
Time System Service Multi-clientThis example application demonstrates the multi-client system timer functionality
USART Driver Asynchronous - USART EchoThis example echoes the received characters over the console using the USART driver in asynchronous mode
USART Driver Synchronous - USART EchoThis example echoes the received characters over the console using the USART driver in synchronous mode