1.15 TCP/IP WEB NET Super Set SDCard FATFS
This application demo enables almost all the Application Layer modules in MPLAB® Harmony 3 TCP/IP Stack. It is also based on Web Net Server SD Card application.
Description
The TCP/IP WEB NET Super Set SDCard FATFS application is based on MPLAB® Harmony 3 TCP/IP Stack.
The Harmony TCP/IP stack is a collection of different network protocols.
The source files of Harmony 3 TCP/IP stack is available here.
The demo is created with MPLAB X IDE and MCC plugin.
MCC Project Graph - TCP/IP WEB NET Super Set SDCard FATFS
The following Project Graph shows the Harmony components included in the TCP/IP WEB NET Super Set SDCard FATFS demo application.

FreeRTOS component is required for RTOS application. For bare-metal (non-RTOS) FreeRTOS component should not be selected.
wolfSSL component is added for secure connection which supports TLS.
wolfCrypt module enabled with MD5 and SHA authentication
FILE SYSTEM is added to read and write from the SDMMC( sdcard ) module with FAT file system.
TCP/IP Configuration - TCP/IP WEB NET Super Set SDCard FATFS
The TCP/IP modules enabled for the demo is shown in the TCP/IP Configuration Overview
More details of TCP/IP Configuration plugin is available here
The Ethernet interface in this demo-configuration use GMAC0 with Onboard Gigabit Ethernet PHY Transceiver LAN8840.

The Ethernet interface in this demo-configuration use GMAC1 with External Gigabit Ethernet PHY Transceiver LAN8840.

The Application Layer modules enabled in the demo are as follows:
- Application Layer Modules
- ANNOUNCE to discover the Microchip devices within a local network.
- Berkeley API provides the Berkeley_Socket_Distribution (BSD) wrapper to the native Harmony TCP/IP Stack APIs.
- DHCP Client to discover the IPv4 address from the nearest DHCP Server.
- DHCP SERVER is used to assign IP addresses to DHCP clients from the configured IP address database.
- DHCPv6 CLIENT module will allow your application to dynamically obtain an IPv6 address from a DHCPv6 server.
- DNS Client provides DNS resolution capabilities to the stack. DNS CLIENT also known as the DNS Resolver, will try to resolve the IP address from its local resources, which includes the Name to Address mappings in the local DNS cache.
- DNS SERVER translate domain names into IP addresses.
- FTP CLIENT module allows application to upload the files to, and download the files from, any FTP server.
- FTP SERVER facilitates the uploading of files to, and downloading of files from, a network device.
- HTTPNET SERVER enables the target board to act as a Web Server for the secured port number 443.
- IPERF implements the iPerf protocol to measure networking bandwidth and performance
- NBNS NetBIOS Name Service protocol associates host names with IP addresses. This assign of human-name host names to access boards on the same subnet.
- SMTP CLIENT let applications send e-mails to any recipient worldwide.
- SNTP Simple Network Time Protocol updates its internal time periodically using a pool of public global time servers.
- TELNET provides bidirectional, interactive communication between two nodes on the Internet or on a Local Area Network.
- TFTP CLIENT module supports reading and writing of files (or mail) from/to a remote server.
- TFTP SERVER is a simple protocol used to transfer files. It waits for client requests to read and write files.
- ZEROCONF, enables devices on an IP network to automatically configure themselves.
Downloading and Building the application
To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file.
This content can also be downloaded using content manager by following these instructions.
Path of the application within the repository is apps\web_net_super_set_sdcard_fatfs\ .
To build the application, refer to the following list of demo configurations and open the project using MPLAB X IDE.
| Project Name | Target Device | Development Board | Description |
|---|---|---|---|
| sam_a7d65_curiosity_gmac0.X | SAMA7D65 | SAMA7D65-Curiosity | TCP/IP WEB NET Super Set SDCard FATFS - Onboard Gigabit Ethernet PHY LAN8840 - Bare Metal |
| sam_a7d65_curiosity_gmac0_freertos.X | SAMA7D65 | SAMA7D65-Curiosity | TCP/IP WEB NET Super Set SDCard FATFS - Onboard Gigabit Ethernet PHY LAN8840 - FreeRTOS |
| sam_a7d65_curiosity_gmac1.X | SAMA7D65 | SAMA7D65-Curiosity+ LAN8840 EDS2 Daughter Card | TCP/IP WEB NET Super Set SDCard FATFS - External Gigabit Ethernet PHY LAN8840 - Bare Metal |
| sam_a7d65_curiosity_gmac1_freertos.X | SAMA7D65 | SAMA7D65-Curiosity+ LAN8840 EDS2 Daughter Card | TCP/IP WEB NET Super Set SDCard FATFS - External Gigabit Ethernet PHY LAN8840 - FreeRTOS |
Hardware Setup - SAMA7D65-Curiosity
The target board for running the application is SAMA7D65-Curiosity.
This section provides essential hardware configuration of this target board to run TCP/IP applications.

Board Setup
To set up the hardware, refer to the section Board Setup in SAMA7D65-Curiosity Kit User Guide.
- Default jumper setting of the board is shown above.
- Connect the USB Type-C cable between USB-A port on the board and host PC. This will supply power to the board.
- Connect a USB-UART converter for console output between the UART DEBUG port on the board and host PC.
- Connect the debugger/programmer between JTAG connector on the board and host PC.
- Insert a microSD card with SD adapter into the SD Card connector(which is on backside of the board) as shown above .
- For GMAC0 application demos, connect Ethernet cable between RJ45 connector of Onboard Gigabit Ethernet PHY LAN8840 and router/switch/computer.
- For GMAC1 application demos, connect Ethernet cable between RJ45 connector of External Gigabit Ethernet PHY LAN8840 (through SODIMM add-on slot) and router/switch/computer.
Setting up at91bootstrap loader
To load the application binary onto the target device, we need to use at91bootstrap loader.
Refer to the at91bootstrap loader documentation for details on how to configure and run/debug the application using MPLABX and booting application using an SD Card.
Running the Application
- Open a terminal application on the host computer (like Hyper-terminal or Tera Term).
- Configure the terminal application for serial port connected to UART DEBUG port.
- Set baud rate as 115200 in the terminal application.
- Build and download the application project on the target board.
- Ensure connection from Gigabit(1000Mbps) capable network socket of a router/switch/computer to the board.
- Ensure SD card is formatted and loaded with the web pages provided within the /net_apps_sama7d6/apps/web_net_server_sdcard_fatfs/src/web_pages directory.
- Insert SD Card to its slot on target board.
- Verify the TCP/IP Stack initialization console messages.

If DHCP client is enabled in the demonstration, wait for the DHCP server to assign an IP address for the development board.
This will be printed on the console. Otherwise, the default static IP address will be assigned to the board.
By entering the command netinfo, the response is obtained as shown above.
Demo Test
- To test the web server functionality, refer Web Net Server demo.
- The command interface is enabled for all the Application Layer modules. These modules can be configured and tested with commands from Console.