1.2.5.4.2 SRV_PCRC_SetSNAValue Function
C
void SRV_PCRC_SetSNAValue
(
uint8_t* sna
);Summary
Sets SNA (Sub-Network Address) value to be used as initial value on further CRC calculations (used by PRIME stack).
Description
This routine sets the value that will be set as the initial CRC value for computations related to PRIME stack, as stated on PRIME specification.
Precondition
None.
Parameters
| Param | Description |
|---|---|
| sna | Pointer to buffer containing SNA value |
Returns
None.
Example
uint8_t sna[PCRC_SNA_SIZE]; SRV_PCRC_SetSNAValue(sna);
Remarks
None.