1.2.11.4.6 CIPHER_Wrapper_AesEaxDecrypt Function
C
int32_t CIPHER_Wrapper_AesEaxDecrypt(uint8_t *data, uint32_t dataLen,
uint8_t *iv, uint32_t ivLen,
uint8_t *aad, uint32_t aadLen,
uint8_t *tag, uint32_t tagLen
uint8_t *key)Summary
Performs AES-EAX authenticated decryption of a buffer.
Description
This function performs AES-EAX encryption of a buffer and authenticates using authentication tag. The size of the key is 16 bytes.
Precondition
None.
Parameters
| Param | Description |
|---|---|
| data | Pointer to buffer holding the input ciphered data. The output plain data is stored in the same buffer |
| dataLen | Length of the input/output data in bytes |
| iv | Pointer to initialization vector (nonce) |
| ivLen | Length of the nonce in bytes |
| aad | Pointer to additional authentication data field |
| aadLen | Length of additional authentication data in bytes |
| tag | Pointer to buffer holding the authentication tag |
| tagLen | Length of the authentication tag in bytes |
| key | Pointer to buffer holding the 16-byte key itself |
Returns
CIPHER_WRAPPER_RETURN_GOOD: Successful decryption.
Any other value: Error in the decryption.
Example
int32_t ret;
uint8_t nonce[] = { some initialization nonce };
uint8_t data[] = { some ciphered message };
uint8_t aad[] = { some additional authentication data };
uint8_t tag[] = { authentication tag received for verification };
uint8_t key[16] = { some key };
ret = CIPHER_Wrapper_AesEaxDecrypt(data, sizeof(data),
nonce, sizeof(nonce),
aad, sizeof(aad),
tag, sizeof(tag),
key);Remarks
None.