2.1.4.42 DRV_MCMETROLOGY_AFE_EVENTS Struct

C
typedefstruct {
    uint16_t swell;
    uint16_t sag;
    uint16_t creep;
    uint16_t phActive;
} DRV_MCMETROLOGY_AFE_EVENTS;
Summary

Identifies all events related to metrology library.

Description

Field description:

  • swell: A bitmap of the Voltage SWELL Detected Flag for Channels (bit 0 corresponds to Channel 0). The result is updated just for the channels configured as voltage. "1" means that voltage Swell x is detected.
  • sag: A bitmap of the Voltage SAG Detected Flag for Channels (bit 0 corresponds to Channel 0). The result is updated just for the channels configured as voltage. "1" means that voltage Sag x is detected.
  • creep: A bitmap of the CREEP Detected Flag for Channel x (bit 0 corresponds to Channel 0). The result is updated just for the channels configured as current. "1" means that voltage Creep x is detected.
  • phActive: A bitmap of the Phase Detected Flag for Channel x (bit 0 corresponds to Channel 0). "1" means that Phase x is active.
Remarks

None.