3.3.2 Using the Library
The EMAFE peripheral library can be used in different ways:
- Direct Transfer: Read data samples from the registers of the EMAFE peripheral
- DMA Transfer: Read a set of data samples from data memory
Direct Transfer
APP_DATA appData; /* Buffer setting */ #define APP_SAMPLE_CHANNELS 1600 // 320 samples/cycle(50Hz) * 5 cycles /** Buffer to store sample sets */ static uint32_t pSamplesBuffer[APP_SAMPLE_CHANNELS] = {0}; void SYS_Initialize ( void* data ) { (...) EMAFE_Initialize(); (...) } void _appEmafeCallback(uint32_t interruptStatus) { if (interruptStatus & EMAFE_ISR_DRDY_Msk) { *appData.pSamplesData++ = EMAFE_GetDataChannel(EMAFE_CHN_2_ID); appData.samplesCounter++; if (appData.samplesCounter == APP_SAMPLE_CHANNELS) { EMAFE_DisableFilter(EMAFE_MR_LPF_ON2_Msk); EMAFE_DisableInterrupt(EMAFE_IDR_DRDY_Msk); appData.newDataReady = true; } } } static void _emafeADCReset(bool enable) { if (enable) { /* Enable ADC SOFT RESET */ EMAFE_ADCEnableSoftReset(); } else { /* Disable ADC SOFT RESET */ EMAFE_ADCDisableSoftReset(); /* Wait SYSRDY */ while (!(EMAFE_ADCIsAnalogSystemReady())); } } static void _emafeConfigADCChannels(bool tempEnable, uint8_t gainI1, uint8_t gainI2) { /* EMAFE Release Reset */ _emafeADCReset(false); /* Enable ADC Channels */ EMAFE_ADCI0Enable(tempEnable); while (!EMAFE_ADCI0IsEnable()); EMAFE_ADCI1Enable(gainI1); while (!EMAFE_ADCI1IsEnable()); EMAFE_ADCV1Enable(); while (!EMAFE_ADCV1IsEnable()); EMAFE_ADCI2Enable(gainI2); while (!EMAFE_ADCI2IsEnable()); EMAFE_ADCV2Enable(); while (!EMAFE_ADCV2IsEnable()); /* Set ADC clock configuration */ EMAFE_ADCSetClockConfig(EMAFE_ADC_CLOCK_FREQRATIO_4, EMAFE_ADC_CLOCK_MCLKDIV_ANACK2); } void APP_Initialize ( void ) { /* Place the App state machine in its initial state. */ appData.state = APP_STATE_ADC_CONTROL_INIT; appData.timer = SYS_TIME_HANDLE_INVALID; appData.pSamplesData = pSamplesBuffer; appData.samplesCounter = 0; appData.newDataReady = false; appData.dataFormat = EMAFE_EMR_FORMAT_FULLRANGE; } void APP_Tasks ( void ) { switch ( appData.state ) { /* Application's initial state. */ case APP_STATE_ADC_CONTROL_INIT: { _emafeConfigADCChannels(true, 0, 0); /* Enable Analog controls. First enable LDO. */ appData.state = APP_STATE_ADC_ENABLE_LDO; SYS_TIME_DelayMS(1, &appData.timer); break; } case APP_STATE_ADC_ENABLE_LDO: { if ((appData.timer == SYS_TIME_HANDLE_INVALID) || (SYS_TIME_DelayIsComplete(appData.timer))) { if (EMAFE_ADCIsLDOEnable()) { appData.state = APP_STATE_ADC_ENABLE_BIAS; appData.timer = SYS_TIME_HANDLE_INVALID; } else { EMAFE_ADCEnableLDO(); SYS_TIME_DelayMS(10, &appData.timer); } } } break; case APP_STATE_ADC_ENABLE_BIAS: { if ((appData.timer == SYS_TIME_HANDLE_INVALID) || (SYS_TIME_DelayIsComplete(appData.timer))) { if (EMAFE_ADCIsBIASEnable()) { appData.state = APP_STATE_ADC_ENABLE_REF; appData.timer = SYS_TIME_HANDLE_INVALID; } else { EMAFE_ADCEnableBIAS(); SYS_TIME_DelayMS(10, &appData.timer); } } } break; case APP_STATE_ADC_ENABLE_REF: { if ((appData.timer == SYS_TIME_HANDLE_INVALID) || (SYS_TIME_DelayIsComplete(appData.timer))) { if (EMAFE_ADCIsREFEnable()) { appData.state = APP_STATE_FILTER_CONTROL_INIT; appData.timer = SYS_TIME_HANDLE_INVALID; } else { EMAFE_ADCEnableREF(); /* Wait 100 ms for VREF setting */ SYS_TIME_DelayMS(100, &appData.timer); } } } break; case APP_STATE_FILTER_CONTROL_INIT: { /* LPFIF reset */ EMAFE_SoftReset(); /* Decimation LPFIF Filters exits the reset state */ EMAFE_SetSincDecimationFiltersReset(false); /* Set DSP clock prescaler ratio */ EMAFE_SetClockPrescalerRatio(EMAFE_EMR_MCLKDIV_LPF_MCLKDIV4_Val); EMAFE_SetDataFormat(appData.dataFormat); EMAFE_SetOSR(EMAFE_EMR_OSR_OSR64_Val); appData.state = APP_STATE_FILTER_START_CAPTURE; SYS_TIME_DelayMS(2, &appData.timer); break; } case APP_STATE_FILTER_START_CAPTURE: { if (SYS_TIME_DelayIsComplete(appData.timer)) { appData.newDataReady = false; appData.samplesCounter = 0; appData.pSamplesData = pSamplesBuffer; /* Register callback */ EMAFE_CallbackRegister(_appEmafeCallback); /* Init Decimation Filters */ EMAFE_EnableFilter(EMAFE_MR_LPF_ON2_Msk); /* Enable Interrupt */ EMAFE_EnableInterrupt(EMAFE_IER_DRDY_Msk); appData.state = APP_STATE_FILTER_PRINT_SAMPLES; } } break; case APP_STATE_FILTER_PRINT_SAMPLES: { if (appData.newDataReady) { appData.pSamplesData = pSamplesBuffer; appData.samplesCounter = 0; appData.newDataReady = false; SYS_TIME_DelayMS(5, &appData.timer); } if (SYS_TIME_DelayIsComplete(appData.timer)) { if (appData.samplesCounter < APP_SAMPLE_CHANNELS) { uint16_t index; for (index = 0; index < APP_SAMPLES_PRINT; index += 5) { uint32_t s0, s1, s2, s3, s4; if (appData.dataFormat == EMAFE_EMR_FORMAT_FULLRANGE_Val) { s0 = *appData.pSamplesData; appData.pSamplesData++; s1 = *appData.pSamplesData; appData.pSamplesData++; s2 = *appData.pSamplesData; appData.pSamplesData++; s3 = *appData.pSamplesData; appData.pSamplesData++; s4 = *appData.pSamplesData; appData.pSamplesData++; } else { s0 = *appData.pSamplesData << 8; appData.pSamplesData++; s1 = *appData.pSamplesData << 8; appData.pSamplesData++; s2 = *appData.pSamplesData << 8; appData.pSamplesData++; s3 = *appData.pSamplesData << 8; appData.pSamplesData++; s4 = *appData.pSamplesData << 8; appData.pSamplesData++; } appData.samplesCounter += 5; SYS_CONSOLE_Print(SYS_CONSOLE_INDEX_0, "%08X\r\n%08X\r\n%08X\r\n%08X\r\n%08X\r\n", s0, s1, s2, s3, s4); } SYS_TIME_DelayMS(100, &appData.timer); } else { appData.state = APP_STATE_FILTER_IDLE; } } } break; case APP_STATE_FILTER_IDLE: default: { /* TODO: Handle error in application's state machine. */ break; } } }
DMA Transfer
APP_DATA appData; /* Buffer setting */ #define APP_SAMPLE_CHANNELS 1600 // 320 samples/cycle(50Hz) * 5 cycles /** Buffer to store sample sets */ static uint32_t pSamplesBuffer[APP_SAMPLE_CHANNELS] = {0}; void SYS_Initialize ( void* data ) { (...) EMAFE_Initialize(); (...) } void _appEmafeCallback(uint32_t interruptStatus) { if (interruptStatus & EMAFE_IER_ENDRX_Msk) { EMAFE_DMATransfer(false, EMAFE_PTCR_RXTDIS_Msk); EMAFE_DisableInterrupt(EMAFE_IDR_ENDRX_Msk); appData.newDataReady = true; } } static void _emafeADCReset(bool enable) { if (enable) { /* Enable ADC SOFT RESET */ EMAFE_ADCEnableSoftReset(); } else { /* Disable ADC SOFT RESET */ EMAFE_ADCDisableSoftReset(); /* Wait SYSRDY */ while (!(EMAFE_ADCIsAnalogSystemReady())); } } static void _emafeConfigADCChannels(bool tempEnable, uint8_t gainI1, uint8_t gainI2) { /* EMAFE Release Reset */ _emafeADCReset(false); /* Enable ADC Channels */ EMAFE_ADCI0Enable(tempEnable); while (!EMAFE_ADCI0IsEnable()); EMAFE_ADCI1Enable(gainI1); while (!EMAFE_ADCI1IsEnable()); EMAFE_ADCV1Enable(); while (!EMAFE_ADCV1IsEnable()); EMAFE_ADCI2Enable(gainI2); while (!EMAFE_ADCI2IsEnable()); EMAFE_ADCV2Enable(); while (!EMAFE_ADCV2IsEnable()); /* Set ADC clock configuration */ EMAFE_ADCSetClockConfig(EMAFE_ADC_CLOCK_FREQRATIO_4, EMAFE_ADC_CLOCK_MCLKDIV_ANACK2); } void APP_Initialize ( void ) { /* Place the App state machine in its initial state. */ appData.state = APP_STATE_ADC_CONTROL_INIT; appData.timer = SYS_TIME_HANDLE_INVALID; appData.pSamplesData = pSamplesBuffer; appData.newDataReady = false; appData.dataFormat = EMAFE_EMR_FORMAT_FULLRANGE; } void APP_Tasks ( void ) { switch ( appData.state ) { /* Application's initial state. */ case APP_STATE_ADC_CONTROL_INIT: { _emafeConfigADCChannels(true, 0, 0); /* Enable Analog controls. First enable LDO. */ appData.state = APP_STATE_ADC_ENABLE_LDO; SYS_TIME_DelayMS(1, &appData.timer); break; } case APP_STATE_ADC_ENABLE_LDO: { if ((appData.timer == SYS_TIME_HANDLE_INVALID) || (SYS_TIME_DelayIsComplete(appData.timer))) { if (EMAFE_ADCIsLDOEnable()) { appData.state = APP_STATE_ADC_ENABLE_BIAS; appData.timer = SYS_TIME_HANDLE_INVALID; } else { EMAFE_ADCEnableLDO(); SYS_TIME_DelayMS(10, &appData.timer); } } } break; case APP_STATE_ADC_ENABLE_BIAS: { if ((appData.timer == SYS_TIME_HANDLE_INVALID) || (SYS_TIME_DelayIsComplete(appData.timer))) { if (EMAFE_ADCIsBIASEnable()) { appData.state = APP_STATE_ADC_ENABLE_REF; appData.timer = SYS_TIME_HANDLE_INVALID; } else { EMAFE_ADCEnableBIAS(); SYS_TIME_DelayMS(10, &appData.timer); } } } break; case APP_STATE_ADC_ENABLE_REF: { if ((appData.timer == SYS_TIME_HANDLE_INVALID) || (SYS_TIME_DelayIsComplete(appData.timer))) { if (EMAFE_ADCIsREFEnable()) { appData.state = APP_STATE_FILTER_CONTROL_INIT; appData.timer = SYS_TIME_HANDLE_INVALID; } else { EMAFE_ADCEnableREF(); /* Wait 100 ms for VREF setting */ SYS_TIME_DelayMS(100, &appData.timer); } } } break; case APP_STATE_FILTER_CONTROL_INIT: { /* LPFIF reset */ EMAFE_SoftReset(); /* Decimation LPFIF Filters exits the reset state */ EMAFE_SetSincDecimationFiltersReset(false); /* Set DSP clock prescaler ratio */ EMAFE_SetClockPrescalerRatio(EMAFE_EMR_MCLKDIV_LPF_MCLKDIV4_Val); EMAFE_SetDataFormat(appData.dataFormat); EMAFE_SetOSR(EMAFE_EMR_OSR_OSR64_Val); appData.state = APP_STATE_FILTER_START_CAPTURE; SYS_TIME_DelayMS(2, &appData.timer); break; } case APP_STATE_FILTER_START_CAPTURE: { if (SYS_TIME_DelayIsComplete(appData.timer)) { /* Register callback */ EMAFE_CallbackRegister(_appEmafeCallback); /* Init Decimation Filters */ EMAFE_EnableFilter(EMAFE_MR_LPF_ON2_Msk); /* Setup DMA */ EMAFE_EnableDMAChannel(EMAFE_MR_DMACH2_Msk); EMAFE_DMATransfer(false, EMAFE_PTCR_RXTDIS_Msk); EMAFE_DMASetup(pSamplesBuffer, APP_SAMPLE_CHANNELS, NULL, 0); EMAFE_DMATransfer(true, EMAFE_PTCR_RXTEN_Msk); /* Enable Interrupt */ EMAFE_EnableInterrupt(EMAFE_IER_ENDRX_Msk); appData.state = APP_STATE_FILTER_PRINT_SAMPLES; } } break; case APP_STATE_FILTER_PRINT_SAMPLES: { if (appData.newDataReady) { appData.newDataReady = false; appData.pSamplesData = pSamplesBuffer; appData.samplesCounter = 0; SYS_TIME_DelayMS(5, &appData.timer); } if (appData.pSamplesData != NULL) { if (SYS_TIME_DelayIsComplete(appData.timer)) { if (appData.samplesCounter < APP_SAMPLE_CHANNELS) { uint16_t index; for (index = 0; index < APP_SAMPLES_PRINT; index += 5) { uint32_t s0, s1, s2, s3, s4; if (appData.dataFormat == EMAFE_EMR_FORMAT_FULLRANGE_Val) { s0 = *appData.pSamplesData; appData.pSamplesData++; s1 = *appData.pSamplesData; appData.pSamplesData++; s2 = *appData.pSamplesData; appData.pSamplesData++; s3 = *appData.pSamplesData; appData.pSamplesData++; s4 = *appData.pSamplesData; appData.pSamplesData++; } else { s0 = *appData.pSamplesData << 8; appData.pSamplesData++; s1 = *appData.pSamplesData << 8; appData.pSamplesData++; s2 = *appData.pSamplesData << 8; appData.pSamplesData++; s3 = *appData.pSamplesData << 8; appData.pSamplesData++; s4 = *appData.pSamplesData << 8; appData.pSamplesData++; } appData.samplesCounter += 5; SYS_CONSOLE_Print(SYS_CONSOLE_INDEX_0, "%08X\r\n%08X\r\n%08X\r\n%08X\r\n%08X\r\n", s0, s1, s2, s3, s4); } SYS_TIME_DelayMS(100, &appData.timer); } else { appData.pSamplesData = NULL; appData.state = APP_STATE_FILTER_IDLE; } } } } break; case APP_STATE_FILTER_IDLE: default: { /* TODO: Handle error in application's state machine. */ break; } } }