3.3.4 Peripheral Library Interface

EMAFE peripheral library provides the following interfaces:

Table 3-4. EMAFE Functions
NameDescription
EMAFE_InitializeInitializes the EMAFE peripheral
EMAFE_ResetResets the EMAFE peripheral by using EMAFE_NRESET GPIO
EMAFE_SoftResetResets the EMAFE peripheral by using peripheral register
EMAFE_SetSincDecimationFiltersResetEnters/exits the reset state of low-pass filters
EMAFE_EnableFilterEnables the corresponding low-pass filter
EMAFE_DisableFilterDisables the corresponding low-pass filter
EMAFE_EnableDMAChannelEnables the corresponding DMA channel
EMAFE_DisableDMAChannelDisables the corresponding DMA channel
EMAFE_GetDataChannelGet the last sample of the corresponding low-pass filter
EMAFE_GetAllDataChannelGet the last samples of all low-pass filters
EMAFE_EnableVariationDetectionEnables the detection of variation of the filtered data
EMAFE_DisableVariationDetectionDisables the detection of variation of the filtered data
EMAFE_IsEnableVariationDetectionCheck if the detection of variation has been enabled
EMAFE_SetDifferenceComparisonModeSet the Comparison mode between two channels
EMAFE_SetDataFormatSet data format of the captured samples
EMAFE_SetClockPrescalerRatioSet the clock prescaler ratio in the low-pass filter
EMAFE_SetOSRSet OSR of the decimation filters
EMAFE_SetComparisonModeChannelASet the Comparison mode between channel A and two thresholds
EMAFE_SetComparisonModeChannelBSet the Comparison mode between channel B and two thresholds
EMAFE_EnableInterruptEnables interrupt flags
EMAFE_DisableInterruptDisables interrupt flags
EMAFE_GetInterruptMaskRead interrupt flags mask
EMAFE_GetInterruptSatusRead interrupt flags status
EMAFE_GetStatusRead comparison events on Channel A and B
EMAFE_WriteProtectionSetSet Write Protection mode
EMAFE_WriteProtectionGetGet Write Protection state
EMAFE_CallbackRegisterSets a callback function that is called when interrupt is raised
Table 3-5. EMAFE ADC Functions
NameDescription
EMAFE_ADCI0EnableEnable ADC I0
EMAFE_ADCI0DisableDisable ADC I0
EMAFE_ADCI0IsEnableCheck if ADC I0 is enabled
EMAFE_ADCI1EnableEnable ADC I1
EMAFE_ADCI1DisableDisable ADC I1
EMAFE_ADCI1IsEnableCheck if ADC I1 is enabled
EMAFE_ADCV1EnableEnable ADC V1
EMAFE_ADCV1DisableDisable ADC V1
EMAFE_ADCV1IsEnableCheck if ADC V1 is enabled
EMAFE_ADCI2EnableEnable ADC I2
EMAFE_ADCI2DisableDisable ADC I2
EMAFE_ADCI2IsEnableCheck if ADC I2 is enabled
EMAFE_ADCV2EnableEnable ADC V2
EMAFE_ADCV2DisableDisable ADC V2
EMAFE_ADCV2IsEnableCheck if ADC V2 is enabled
EMAFE_ADCSetClockConfigSet ADC clocks configuration
EMAFE_ADCEnableBIASEnable Current Bias Generator
EMAFE_ADCDisableBIASDisable Current Bias Generator
EMAFE_ADCIsBIASEnableCheck if Current Bias Generator is enabled
EMAFE_ADCEnableREFEnable Voltage Reference
EMAFE_ADCDisableREFDisable Voltage Reference
EMAFE_ADCIsREFEnableCheck if Voltage Reference is enabled
EMAFE_ADCEnableLDOEnable internal LDO
EMAFE_ADCDisableLDODisable internal LDO
EMAFE_ADCIsLDOEnableCheck if internal LDO is enabled
EMAFE_ADCIsAnalogSystemReadyCheck if analog system is ready
EMAFE_ADCEnableSoftResetSet ADCs in reset state
EMAFE_ADCDisableSoftResetExits the ADCs reset state
EMAFE_ADCSetSecurityControlsConfigure the security options of the analog system
EMAFE_ADCGetSecurityControlsGet the security options of the analog system
EMAFE_ADCGGetVREFLowTempGet the Voltage Reference at low temperature
EMAFE_ADCGGetTEMPLowTempGet the Temperature Sensor at low temperature
EMAFE_ADCGGetVREFHighTempGet the Voltage Reference at high temperature
EMAFE_ADCGGetTEMPHighTempGet the Temperature Sensor at high temperature
Table 3-6. EMAFE Types
NameTypeDescription
EMAFE_STATUSEnumIdentifies the EMAFE status
EMAFE_CHANNEL_IDEnumIdentifies the EMAFE channel
EMAFE_COMP_CHANNEL_IDEnumIdentifies the channel used to perform a comparison
EMAFE_DIFF_COMPARISON_TYPEEnumIdentifies the type of comparison between two channels
EMAFE_DIFF_COMPARISON_DATAStructDescribes the data used to perform a comparison between two channels
EMAFE_CONDITION_TYPEEnumIdentifies the condition applied for detection on channel A/B
EMAFE_COMPARISON_DATAStructDescribes the data used to perform a comparison between one channel and threshold