1.17 QSPI Flash Read Write
This example shows how to use the QSPI Peripheral library to perform erase, write and read operation with the QSPI Serial Flash memory in Quad IO mode.
Description
This example uses the QSPI peripheral library to erase and write an array of values to the QSPI Serial Flash memory. It verifies the value written by reading the values back and comparing it to the value written.
Downloading and Building the Application
To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.
Path of the application within the repository is apps/qspi/qspi_read_write/firmware.
To build the application, refer to the following table and open the project using its IDE.
| Project Name | Description | 
|---|---|
| pic32cz_ca70_curiosity_ultra.X | MPLABX project for PIC32CZ CA70 Curiosity Ultra Development Kit | 
Setting Up the Hardware
The following table shows the target hardware for the application projects.
| Project Name | Description | 
|---|---|
| pic32cz_ca70_curiosity_ultra.X | PIC32CZ CA70 Curiosity Ultra Development Kit | 
Setting Up PIC32CZ CA70 Ultra Curiosity Development Kit
- Connect the Debug USB port on the board to the computer using a micro USB cable
 
Running the Application
- Build and Program the application using its IDE
 - LED indicates success or failure:
- The LED will blink when the value read from the QSPI Serial Flash memory matched with the written value
 - The LED is turned ON when the value read from the QSPI Serial Flash did not match with the written value
 
 
| Board | LED Name | 
|---|---|
| PIC32CZ CA70 Curiosity Ultra Development Kit | LED0 |