1.2 AFEC Polling
This example uses AFEC peripheral library to sample an analog input in polled mode and send the converted data to console.
Description
In this example, the DAC output is fed to the ADC input. The DAC output is changed by 0.1V when switch is pressed. The ADC conversion is triggered by software and converted result is displayed on the console.
Downloading and Building the Application
To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.
Path of the application within the repository is apps/afec/afec_polled_mode/firmware.
To build the application, refer to the following table and open the project in their respective IDEs.
| Project Name | Description | 
|---|---|
| pic32cz_ca70_curiosity_ultra.X | MPLABX project for PIC32CZ CA70 Curiosity Ultra Development Kit | 
Setting Up the Hardware
The following table shows the target hardware for the application projects.
| Project Name | Description | 
|---|---|
| pic32cz_ca70_curiosity_ultra.X | PIC32CZ CA70 Curiosity Ultra Development Kit | 
Setting Up PIC32CZ CA70 Ultra Curiosity Development Kit
- An analog input (AD0) is fed from the DAC output. DAC output is incremented by 0.1 V on Switch (SW0) press
 - An analog input "AD0" is mapped to Port Pin "PB1" that is routed to "Pin 14 of the EXT1 header"
 - The DAC output "DAC0" is mapped to Port Pin "PB13" that is routed to "Pin 8 of the EXT2 header"
 - Use a jumper wire to connect "Pin 14 of the EXT1" to "Pin 8 of the EXT2"
 - Connect 3.3V from pin 4 of J401 to VREFIN pin on J302. This generates 2.048V reference voltage (VREFP) for the DAC.
 - Connect GND from pin 6 of J401 to GND pin on J302.
 - Connect the Debug USB port on the board to the computer using a micro USB cable
 
Running the Application
- Open the Terminal application (Ex.:Tera term) on the computer
 - Connect to the PICkit4 On Board
                    Virtual COM port and configure the serial settings as follows:
- Baud : 115200
 - Data : 8 Bits
 - Parity : None
 - Stop : 1 Bit
 - Flow Control : None
 
 - Build and Program the application using its respective IDE
 - The console displays the ADC Count and the ADC Input Voltage
 - Press the switch to change the DAC output by 0.1 V from 0 V to 2.048 V
 - Observe the ADC input value and the respective ADC count value
 - Note that the VREFP for both DAC and AFEC modules is 2.048V. As a result, the DAC and AFEC output will saturate at 2.048V.
 
                
| Board | Switch Name | 
|---|---|
| PIC32CZ CA70 Curiosity Ultra Development Kit | SW0 |