4.6.2 Functions
static void DeviceResetCheck (void)
Checks and performs a reset when required.
static void ParserDataReset (void)
Resets parser data use for command reception.
static bool SequenceNumberValidate (void)
Validates the sequence number of the incoming command.
static void ClientInfoResponseSet (void)
Sets the Get Client Info data in the response buffer.
static bl_result_t OperationalBlockExecute (void)
Processes and executes the FTP command data received by the host.
static void ResponseSet (uint8_t *buffer, uint8_t *responsePayload, ftp_response_status_t responseStatus, uint8_t sequenceByte, uint16_t responsePayloadLength)
Sets the response in the FTP process frame.
static uint8_t TLVAppend (uint8_t *dataBufferStart, ftp_tlv_t *tlvData)
Appends a TLV (Type-Length-Value) structure to a data buffer.
static ftp_abort_code_t AbortCodeGet (bl_result_t targetStatus)
Converts the given result codes into MDFU protocol defined data values.
bl_result_t FTP_Task (void)
Acts as the main task runner of the FTP process. This function will be called in a loop to receive commands from the host and make calls to the responsible software layers to facilitate the device firmware update.
bl_result_t FTP_Initialize (void)
Performs the initialization actions required to set up the FTP and dependent layers.