2.3.3.3 COM_Initialize()
com_adapter_result_t COM_Initialize (uint16_t maximumBufferLength)
Performs initialization actions for the communication peripheral and adapter code.
| in | maximumBufferLength |
- Maximum length that the COM adapter is allowed to read |
COM_PASS - Specified arguments are valid and initialization was successful COM_INVALID_ARG - Specified arguments were invalid COM_FAIL - Error occurred in the SERCOM initialization |
| in | maximumBufferLength |
- Maximum length that the COM adapter is allowed to read |
COM_PASS - Specified arguments were valid and initialization was successful COM_INVALID_ARG - Specified arguments were invalid COM_FAIL - An error occurred in the SERCOM initialization |