2.3.3.1 COM_FrameSet()

com_adapter_result_t COM_FrameSet (const uint8_t * responseBufferPtr, uint16_t responseLength)

Transfers bytes from the given buffer using the defined framing format.

Parameters:
in responseBufferPtr

- Pointer to the buffer that needs to be sent

in responseLength

- Length of the response that needs to be sent

Returns:

COM_PASS - Buffer was transferred without error  

COM_FAIL - An error occurred in SERCOM while transferring the buffer