2.4.3.1 COM_FrameSet()

com_adapter_result_t COM_FrameSet (uint8_t * responseBufferPtr, uint16_t responseLength)

Copies and formats bytes from the given buffer into the static send buffer using the defined framing format.

Note:

For UART, this function will simply send the bytes out of the peripheral because the communication layer does not need to wait for the host to initiate any transfers. Doing this makes it so we do not need to define a static buffer in the communication code.

Parameters:
in responseBufferPtr

- Pointer to the buffer that needs to be sent

in responseLength

- Length of the response that needs to be sent

Returns:

COM_PASS - Buffer was transferred without error  

COM_FAIL - An error occurred in the SERCOM while transferring the buffer  

Copies and formats bytes from the given buffer into the static send buffer using the defined framing format.

Parameters:
in responseBufferPtr

- Pointer to the buffer that needs to be sent

in responseLength

- Length of the response that needs to be sent

Returns:

COM_PASS - Buffer was transferred without error  

COM_FAIL - An error occurred in the SERCOM while transferring the buffer