1 Theory of Operation

Figure 1-1. Simplified Circuit of PFC with Y-Capacitors and Current Source Scheme

Figure 1-1 illustrates the simplified circuit of the Power Factor Correction (PFC) stage connected to an electronic load. CY-PFC is the Y-capacitance of the PFC board (between Neutral and PE), and CY-LOAD is the Y-capacitance of the electronic load (between PGND and PE). The voltage between Neutral and PGND alternates between VOUT and 0V, depending on the polarity of the AC voltage.

During the positive AC half-wave, Q4 is on and Q3 is off, so N is connected to PGND. Conversely, during the negative AC half-wave, Q3 is on and Q4 is off, so N is connected to VOUT.

To manage the charge redistribution of the Y-capacitors, the current source scheme is added to the circuit. At the AC zero crossing, when transitioning from positive to negative current, GPIO_Y_H switches on for a brief period while GPIO_Y_L remains off, thus activating the upper current source. Conversely, during the zero-crossing transition from negative to positive current, GPIO_Y_L switches on for a short period while GPIO_Y_H remains off, thereby activating the lower current source.