Introduction
| Author: Cristina Ionescu, Microchip Technology Inc. |
An embedded system is capable of exchanging stimuli with the outside world using General-Purpose Input/Output (GPIO) ports. GPIO pins are clustered in PORTs and the PIC18 devices provide multiple PORT modules.
This technical brief explains the concepts behind PORT modules and their functionality on the PIC18 family of microcontrollers by implementing the use cases presented below.
- GPIO Read/Write
Example:
This example shows how to read an input pin value, changed by pressing a button, and how to set an output pin value in order to turn an LED on and off.
- Using GPIO Interrupts:
This example shows how to enable the Interrupt-on-Change (IOC). The IOC is configured to be triggered on the falling edge detected on the desired input pin.
- Wake-Up from Sleep:
This example shows how to reduce power consumption by enabling Sleep mode on the device and waking it up using the IOC, with a button controlling the input pin value.
There are two different implementations for each use case that have the same functionalities: one code generated with MPLAB® Code Configurator (MCC) and one bare metal code. The MCC-generated code offers hardware abstraction layers that ease the use of the code across different devices from the same family. The bare metal code is easier to follow, allowing a fast ramp-up on the use case associated code.