The Following Files are added to the RFD project section -
Figure 4-92.
Copy the following folder from the Repo link:(to be mentioned) and paste in the
project path : ble_mac_prov_rfd\firmware\src
Figure 4-93.
Figure 4-94.
Figure 4-95.
Figure 4-96.
Figure 4-97.
Figure 4-98.
Figure 4-99.
Figure 4-100.
Figure 4-101.
Import the app_adv.c and app_adv.h files into the project folder and copy the files
there in order to enable the advertisement service.
Figure 4-102.
Right-click on the Source Files option and select “Add Existing
Item”
Figure 4-103.
In the select item window browse and select the app_adv.c file, and select “C++
Source Files” on the Files of Type option
Figure 4-104.
Now the app_adv.c file is added to the project location. The procedure is the same for
app_adv.h; the only difference is to select the “Header Files option” on the files of
type while choosing the file.