4.2 Getting Started with MCHPRT3 PIC32CX-BZ2 GUI
Program the sample before use of the MCHPRT3 tool. For more details on the HUT code programming process, refer to MPLAB X IDE HUT Code Programming Process .
To run an RF test on the PIC32 WBZ451 Curiosity Board, perform the following procedure:
- Connect the Micro USB in the Curiosity Board to the PC.
- Check whether the jumper for the current measurement was inserted or not.
- Run
MCHPRT3.exe. - From the “Select GUI” drop-down list, select PIC32CX-BZ2.
- Click Open to launch the PIC32CX-BZ2 window.
- Select the respective “COM PORT” (check device manager in PC). A different USB-to-UART serial converter requires the corresponding driver; install accordingly.
- Baud Rate - 115200 (default value)
- Click Connect.
- Click Reset to reset the device. The PIC32 WBZ451 Curiosity Board is ready for RF Test, Calibration and MAC Address Programming.