15 MPLAB® XC32 Object Archiver/Librarian
The MPLAB XC32 Object Archiver/Librarian creates, modifies and
extracts files from archives. This tool is one of several utilities (xc32-ar). An “archive” is a single file
holding a collection of other files in a structure that makes it possible to retrieve
the original individual files (called “members” of the archive).
The original files’ contents, mode (permissions), timestamp, owner and group are preserved in the archive, and can be restored on extraction.
The XC32 archiver/librarian can maintain archives whose
members have names of any length; however, if an f modifier is used,
the file names will be truncated to 15 characters.
The archiver is considered a binary utility because archives of this sort are most often used as “libraries” holding commonly needed subroutines.
The archiver creates an index to the symbols defined in relocatable object modules in the
archive when you specify the modifier s. Once created, this index is
updated in the archive whenever the archiver makes a change to its contents (save for
the q update operation). An archive with such an index speeds up
linking to the library and allows routines in the library to call each other without
regard to their placement in the archive.
You may use xc32-nm -s or
xc32-nm --print-armap
to list this index table. If an archive lacks the table, another form of the XC32 archiver/librarian called xc32-ranlib can be used to add
only the table.
The XC32 archiver/librarian is designed to be
compatible with two different facilities. You can control its activity using command
line options or, if you specify the single command line option -M, you
can control it with a script supplied via standard input.