15.6 Scripts
If you use the single command line option -M with the
archiver, you can control its operation with a rudimentary command language.
xc32-ar -M [ <SCRIPT
]
This form of the MPLAB XC32
archiver/librarian operates interactively if standard input is coming directly from a
terminal. During interactive use, the archiver prompts for input (the prompt is AR
>), and continues executing even after errors. If you redirect standard
input to a script file, no prompts are issued, and the XC32 archiver/librarian abandons execution (with a nonzero exit code) on any
error.
The archiver command language is not designed to be equivalent to the command line options; in fact, it provides somewhat less control over archives. The only purpose of the command language is to ease the transition to the XC32 archiver/librarian for developers who already have scripts written for the MRI “librarian” program.
The syntax for the XC32 archiver/librarian command language is straightforward:
- commands are recognized in upper or lower case; for example,
LISTis the same aslist. In the following descriptions, commands are shown in upper case for clarity. - a single command may appear on each line; it is the first word on the line.
- empty lines are allowed, and have no effect.
- comments are allowed; text after either of the characters “*” or “;” is ignored.
- Whenever you use a list of names as part of the argument to an xc32-ar command, you can separate the individual names with either commas or blanks. Commas are shown in the explanations below, for clarity.
- “+” is used as a line continuation character; if “+” appears at the end of a line, the text on the following line is considered part of the current command.
The table below shows the commands you can use in archiver scripts, or when using the archiver interactively. Three of them have special significance.
| Option | Function |
|---|---|
OPEN or
CREATE | Specify a “current archive”, which is a temporary file required for most of the other commands. |
SAVE | Commits the changes so far specified by the
script. Prior to SAVE, commands affect only the temporary copy
of the current archive. |
ADDLIB
ARCHIVE
| Add all the contents of
ARCHIVE (or, if specified, each named
MODULE from
ARCHIVE) to the current archive.Requires prior use of |
ADDMOD MEMBER,
MEMBER, ... MEMBER | Add each named
MEMBER as a module in the current
archive.Requires prior use of |
CLEAR | Discard the contents of the current archive,
canceling the effect of any operations since the last SAVE.
May be executed (with no effect) even if no current archive is
specified. |
CREATE
ARCHIVE | Creates an archive, and makes it the current
archive (required for many other commands). The new archive is created with a
temporary name; it is not actually saved as
ARCHIVE until you use
SAVE. You can overwrite existing archives; similarly, the
contents of any existing file named ARCHIVE
will not be destroyed until SAVE. |
DELETE MODULE,
MODULE, ... MODULE | Delete each listed
MODULE from the current archive;
equivalent to xc32-ar -d
ARCHIVE
MODULE ... MODULE.Requires prior use of |
DIRECTORY ARCHIVE
(MODULE, ... MODULE)
[OUTPUTFILE] | List each named
MODULE present in
ARCHIVE. The separate command
VERBOSE specifies the form of the output: when verbose
output is off, output is like that of xc32-ar -t ARCHIVE
MODULE.... When verbose output is on, the listing
is like xc32-ar -tv
ARCHIVE
MODULE....Output normally goes
to the standard output stream; however, if you specify
|
END | Exit from the archiver with a 0 exit code to
indicate successful completion. This command does not save the output file; if
you have changed the current archive since the last SAVE
command, those changes are lost. |
EXTRACT MODULE,
MODULE, ... MODULE | Extract each named
MODULE from the current archive,
writing them into the current directory as separate files. Equivalent to
xc32-ar -x
ARCHIVE
MODULE....Requires prior use
of |
LIST | Display full contents of the current archive,
in “verbose” style regardless of the state of VERBOSE. The
effect is like xc32-ar tv
ARCHIVE. (This single command is a XC32 archiver/librarian enhancement, rather
than present for MRI compatibility.)Requires prior use of
|
OPEN
ARCHIVE | Opens an existing archive for use as the
current archive (required for many other commands). Any changes as the result
of subsequent commands will not actually affect
ARCHIVE until you next use
SAVE. |
REPLACE MODULE,
MODULE, ... MODULE | In the current archive, replace each existing
MODULE (named in the
REPLACE arguments) from files in the current working
directory. To execute this command without errors, both the file, and the
module in the current archive, must exist.Requires prior
use of |
VERBOSE | Toggle an internal flag governing the output
from DIRECTORY. When the flag is on,
DIRECTORY output matches output from xc32-ar -tv .... |
SAVE | Commits your changes to the current archive
and actually saves it as a file with the name specified in the last
CREATE or OPEN command.Requires prior use of |