6.2 Contents
The listing files produced by the assembler are composed of the several elements. The example below shows a sample listing file.
The example listing file contains these elements:
- Header – contains the name of the assembler, the name of the
file being assembled, and a page number. This is not shown if the
-anoption is specified. - Title Line – contains the title specified by the
.titledirective. This is not shown if the-anoption is specified. - Subtitle – contains the subtitle specified by the
.sbttldirective. This is not shown if the-anoption is specified. - High-level source if the
-ahoption is given to the assembler. The format for high-level source is:<line #>:<filename> **** <source>For example:
1:hello.c **** #include <stdio.h> - Assembler source if the
-aloption is given to the assembler. The format for assembler source is:<line #> <addr> <encoded bytes> <source>For example:
13 000004 02 00 00 D4 rcall _putsNote:- Line numbers may be repeated.
- Addresses are relative to sections in this module and are not absolute.
- Instructions are encoded in “little endian” order.
- Symbol table if the
-asoption is given to the assembler. Both, a list of defined and undefined symbols will be given. The defined symbols will have the format:DEFINED SYMBOLS <filename>:<line #> <section>:<addr> <symbol>For example:
DEFINED SYMBOLS foo.s:229 .text:00000000 _mainThe undefined symbols will have the format:
UNDEFINED SYMBOLS <symbol>For example:
UNDEFINED SYMBOLS printf
Sample Assembler Listing File
MPLAB XC32 ASSEMBLY Listing: example.1.1.s page 1
Sample PIC32A Assembler Source Code
For illustration only.
1 .title " Sample PIC32A Assembler Source Code"
2 .sbttl " For illustration only."
3
4 .section .const,code
5 hello:
6 000000 48 65 6C 6C .ascii "Hello, World!\n"
6 6F 2C 20 57
6 6F 72 6C 64
6 21 0A
7 00000e 00 00
8 .text
9 .global __reset
10 __reset:
11 000000 03 00 00 80 mov.l #hello,w0
12 000004 02 00 00 D4 rcall _puts
13 000008 01 72 return
14
15 00000a 00 00 .end
MPLAB XC32 ASSEMBLY Listing: example.1.1.s page 2
Sample PIC32A Assembler Source Code
For illustration only.
DEFINED SYMBOLS
*ABS*:0000000000000001 __32AK1216GC41064
*ABS*:0000000000000001 __PIC32A
*ABS*:0000000000000001 __HAS_DSP
*ABS*:0000000000000001 __HAS_DMAV2
*ABS*:0000000000000005 __TARGET_DIVIDE_CYCLES16
*ABS*:0000000000000009 __TARGET_DIVIDE_CYCLES32
*ABS*:0000000000000001 __HAS_AA
*ABS*:0000000000000001 __HAS_ISA32
*ABS*:0000000000000001 __C30ELF
example.1.1.s:5 .const:0000000000000000 hello
example.1.1.s:10 .text:0000000000000000 __reset
UNDEFINED SYMBOLS
_puts