10.3.1 Processor and Startup Modules
The first several lines of a linker script define the processor and startup modules:
OUTPUT_ARCH("32AK1216GC41064")
CRT0_STARTUP(crt0_extendedaa.o)
CRT1_STARTUP(crt1_extendedaa.o)
/*
* Define how to startup, by default we initialize
* everything as normal; change to crt_start_mode to
* preserve preserved data on a restart
*
* Or define your own __crt_start_mode fucntion
*/
CRT_STARTMODE(crt_start_mode_normal)
OPTIONAL(-lp32AK1216GC41064)
OPTIONAL(-lfx)
The OUTPUT_ARCH command specifies the
target processor. The CRTn_STARTUP
commands specify two C run-time startup modules to be loaded from archives. The linker will
select one of these based on whether data initialization has been enabled.
The CRT_STARTMODE command specifies whether data sections marked
"preserved" should be initialized upon startup. This command is bracketed by a preprocessor
expression because some legacy linkers do not support this command.
The OPTIONAL commands specify device-specific libraries that should be
opened if available. If the library file cannot be found, the link will continue without
error unless there are unresolved references in the application.