14.3.3 Objdump Options
The long and short forms of options, shown in the following table, as
alternatives, are equivalent. At least one of the following options -a, -d, -D, -f, -g, -h, -H, -i, -r, -S, -t, -V or -x must be given.
| Option | Function |
|---|---|
-a
| If any of the OBJFILE files are archives, display the
archive header information (in a format similar to ls
-l). Besides the information you could list with xc32-ar tv, xc32-objdump -a shows the
object file format of each archive member. |
-b
format
| Specify the target object file format. The option -b
binary, fr example, allows the utility to work on a raw binary
file. |
-d
| Display the assembler mnemonics for the
machine instructions from OBJFILE. This option only disassembles those
sections that are expected to contain instructions. |
-D
| Like -d, but disassemble the contents of all sections, not just those expected to contain instructions. |
-f
| Display summary information from the overall
header of each of the OBJFILE files. |
--file-start-context | Specify that when displaying inter-listed
source code/disassembly (assumes -S) from a
file that has not yet been displayed, extend the context to the start of the
file. |
-g
| Display debugging information. This attempts to parse debugging information stored in the file and print it out using a C like syntax. Only certain types of debugging information have been implemented. |
-h
| Display summary information from the section
headers of the object file. File segments may be relocated
to nonstandard addresses, for example by using the |
-H
| Print a summary of the options to xc32-objdump and exit. |
-i
| Print a list of the object formats and architectures supported and exit. |
-j name
| Display information only for section
name. |
-l
| Label the display (using debugging information) with the filename and source line numbers corresponding to the object code or relocs shown. Only useful with -d, -D or -r. |
-m
arch
| Specify the target architecture. |
-M
options
| Pass target specific information to the
disassembler. The following options are supported:
|
-P,
| Display object format specific contents |
--prefix-addresses | When disassembling, print the complete address on each line. This is the older disassembly format. |
-r
| Print the relocation entries of the file. If used with -d or -D, the relocations are printed interspersed with the disassembly. |
-s
| Display the full contents of any sections requested. |
-S
| Display source code intermixed with disassembly, if possible. Implies -d. |
--show-raw-insn | When disassembling instructions, print the instruction in hex, as well as in symbolic form. This is the default except when --prefix-addresses is used. |
--no-show-raw-insn | When disassembling instructions, do not print the instruction bytes. This is the default when --prefix-addresses is used. |
--start-address=address | Start displaying data at the specified address. This affects the output of the -d, -r and -s options. |
--stop-address=address | Stop displaying data at the specified address. This affects the output of the -d, -r and -s options. |
-t
| Print the symbol table entries of the file.
This is similar to the information provided by the xc32-nm program. |
-V
| Print the version number of xc32-objdump and exit. |
-w
| Format some lines for output devices that have more than 80 columns. |
-x
| Display all available header information, including the symbol table and relocation entries. Using -x is equivalent to specifying all of -a -f -h -r -t. |
-z
| Normally the disassembly output will skip blocks of zeros. This option directs the disassembler to disassemble those blocks, just like any other data. |