5.5.2 Fill Directive
The .fill repeat[, size[,
value]] directive reserves space for
repeat copies of a
size-byte value derived from
value. The repeated value is the lowest
size bytes of a number sequence consisting of the
highest order 4 bytes being zero and the lowest order 4 bytes being
value rendered in little-endian byte-order.
The size and value
arguments are optional. When not specified, the size
defaults to the value 1 and the value argument defaults
to value 0.
The repeat argument is mandatory and may be zero or more,
but if it is more than 8, then it is deemed to have the value 8.
For example, the following code will place down 3 copies of the byte
0xFF.
.text
.fill 0x3, 1, 0xFF
.align 2
mylabel: b .